2024-02-14 5:34 AM - edited 2024-02-14 5:38 AM
These two notifications refer to the exact same post:
He couldn't have mentioned me without making a reply, so I really don't need two separate notifications!
EDIT
And why are the two email notifications sent 7 minutes apart?!
2024-02-19 3:57 AM
Hi @Andrew Neil,
Thanks for your feedback.
Given that the notifications are triggered separately there is no immediate fix/workaround to this issue.
We can look into scenarios where only one notification is necessary in general. I can't promise we can change anything soon, but the feedback is noted.
Best regards,
Laurids
2024-07-31 10:14 AM
@Laurids_PETERSEN wrote:the notifications are triggered separately the
Why?
Here we see that notifications can be combined:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.