2023-06-22 3:39 AM - edited 2023-06-22 6:29 AM
See ability to upvote until I log in, then disappears.
Seems to impact my view on PC and Phone browsers. I can see people have clicked the Kudos button on my posts in the alerts, so working for some.
For some reason, I can't bold the Subject/Title of this post, so it looks different to others on the page.
Solved! Go to Solution.
2023-06-30 9:13 AM
Millions of settings I don't need, none that improve the utilization of screen real-estate.
2023-06-22 2:18 PM
When it logs me out I see the button again. And I get one chance to click where it logs me in, uprates the posts, but doesn't show me the button or count again..
Others are uprating my posts, so not sure of others experiences with the button/count disappearing..
2023-06-23 4:47 AM
Hi @Tesla DeLorean,
I tested on mobile (iPhone), and desktop (Microsoft edge) and the kudos button is working for me as expected:
To better understand the issue on your end: is the kudos button not visible at all for you when being logged in? Or do you see it but it is greyed out, so you are not able to interact with it?
Also, any further browser details might help to track down the issue.
Thanks,
Amelie
2023-06-23 10:03 AM
Not visible on Android or Chrome (PC) when logged in.
See it before, and can give one up vote as logging in, but then not visible
2023-06-23 10:13 AM
Something about my account, issue also in Edge which I never use, so not adblocker or ghostery..
2023-06-29 12:04 AM - edited 2023-06-30 5:53 AM
Hello @Tesla DeLorean,
thanks for providing further details. I reported the case to the IT team to further investigate and fix it. I will keep you updated if there is any news or feedback on the IT ticket.
Please apologize if this causes any difficulties in the meantime.
Best,
Amelie
2023-06-30 2:11 AM - edited 2023-06-30 5:53 AM
Hello @Tesla DeLorean,
The IT team unfortunately cannot reproduce this case. They suggested to setup a call. I will send you a PM to further discuss the next steps.
Best,
Amelie
2023-06-30 8:58 AM
Looks to be an option buried deep in the user settings / preferences.
2023-06-30 9:13 AM
Millions of settings I don't need, none that improve the utilization of screen real-estate.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.