cancel
Showing results for 
Search instead for 
Did you mean: 

Feature request for the forum: text files view with line numbers

Pavel A.
Super User

When viewing text file attachments, showing line numbers can be helpful. Then we can refer to the line numbers in replies, etc.

 

2 REPLIES 2
Lina_DABASINSKAITE
Community manager

Thanks for the suggestion, @Pavel A. ! 

Curious to see if this would be useful also for others? If it resonates, we can look into feasibility of this feature. 

Thanks a lot,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Could be useful.

See also: Line numbers in source code blocks.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.