cancel
Showing results for 
Search instead for 
Did you mean: 

Attachment access and image viewing issues

TDK
Super User

The "Virus scan in progress..." message is gone, but attachments are still behaving funny.

Issue 1: 2 out of the 3 attachments here cannot be accessed. Clicking on them does nothing and the "download" icon is missing.

https://community.st.com/t5/others-stm32-mcus-related/facing-difficulties-in-interfacing-stm32l433-mcu-to-vcnl4040-i2c/m-p/861339

TDK_0-1766113643986.png

 

Issue 2: I've also noticed that image attachments can't be viewed directly in the past week or so.

Trying to click on the png attached here shows an error instead of showing the image.

TDK_2-1766113825278.png

TDK_1-1766113792498.png

https://community.st.com/t5/stm32-mcus-products/stm32l433rct-freezing-lock-up-problem/m-p/865559/highlight/true#M290358

The download icon works and once downloaded the images can be viewed directly. They appear to be valid PNG files.

 

Seems forum functionality is going backwards. Split this to a new thread if you want. Seems related IMO.

If you feel a post has answered your question, please click "Accept as Solution".
3 REPLIES 3
Lina_DABASINSKAITE
Community manager

Thank you, @TDK , for sharing this information. I have escalated the issue to the troubleshooting team.
I apologize for the inconvenience in the meantime.

Best regards,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Super User

Yes, I have seen this recently.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

Another today here:

AndrewNeil_0-1766397159842.pngAndrewNeil_1-1766397181431.png

https://community.st.com/t5/stm32cubeide-mcus/resolved-stm32cubeide-project-creation-issue/m-p/866247/highlight/true#M40203

 

If I download it, the downloaded file opens OK locally.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.