cancel
Showing results for 
Search instead for 
Did you mean: 

Are other components of CAN datalines robust enough versus ESD?

LauraCx
ST Employee

Are other components of CAN datalines, like termination resistors or capacitors, robust enough versus ESD?

Yes these discrete components are also vulnerable to ESD and their value or lifetime can be impacted by repetitive ESD surges.
But as the CAN protection device must be placed right after the connector, it will protect all the discrete components of the CAN line on top of the CAN transceiver.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.

Version history
Last update:
‎2022-09-16 2:44 AM
Updated by: