2020-06-17 5:29 PM
Analyzing model
C:/Users/Hector Gonzalez/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.1.1/Utilities/windows/stm32ai analyze --name network -m C:/Users/Hector Gonzalez/Desktop/classification_model.h5 --type keras --compression 1 --verbosity 1 --workspace C:\Users\HECTOR~1\AppData\Local\Temp\mxAI_workspace11378610577003599069257813762485 --output C:\Users\Hector Gonzalez\.stm32cubemx\stm32ai_output
Neural Network Tools for STM32 v1.3.0 (AI tools v5.1.1)
TOOL ERROR: Nor Keras nor tf.keras installed.
Creating report file C:\Users\Hector Gonzalez\.stm32cubemx\stm32ai_output\network_analyze_report.txt
IO ERROR: Nor Keras nor tf.keras installed.
Exec/report summary (analyze dur=-0.00s err=-1)
------------------------------------------------------------------------------------------------------------------------
error : IO ERROR: Nor Keras nor tf.keras installed.
model file : C:\Users\Hector Gonzalez\Desktop\classification_model.h5
Nor Keras nor tf.keras installed.
Using TensorFlow backend.
Using TensorFlow backend.
Using TensorFlow backend.
2020-06-17 8:19 PM
This I get when this stm32ai --tools-version command is executed
C:\Users\Hector Gonzalez>stm32ai --tools-version
Using TensorFlow backend.
Traceback (most recent call last):
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow.py", line 58, in <module>
from tensorflow.python.pywrap_tensorflow_internal import *
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 28, in <module>
_pywrap_tensorflow_internal = swig_import_helper()
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 24, in swig_import_helper
_mod = imp.load_module('_pywrap_tensorflow_internal', fp, pathname, description)
File "imp.py", line 242, in load_module
File "imp.py", line 342, in load_dynamic
ImportError: DLL load failed: Error en una rutina de inicialización de biblioteca de vínculos dinámicos (DLL).
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "stm32ai.py", line 510, in <module>
File "stm32ai.py", line 490, in main
File "stm32ai.py", line 430, in setup_cli
File "stm32ai.py", line 193, in early_update_args
File "stm32ai.py", line 138, in tools_version
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\__init__.py", line 3, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\utils\__init__.py", line 6, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\utils\conv_utils.py", line 9, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\backend\__init__.py", line 1, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\backend\load_backend.py", line 90, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\keras\backend\tensorflow_backend.py", line 5, in <module>
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow\__init__.py", line 98, in <module>
from tensorflow_core import *
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\__init__.py", line 40, in <module>
from tensorflow.python.tools import module_util as _module_util
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow\__init__.py", line 50, in __getattr__
module = self._load()
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow\__init__.py", line 44, in _load
module = _importlib.import_module(self.__name__)
File "importlib\__init__.py", line 126, in import_module
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\__init__.py", line 49, in <module>
from tensorflow.python import pywrap_tensorflow
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow.py", line 74, in <module>
raise ImportError(msg)
ImportError: Traceback (most recent call last):
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow.py", line 58, in <module>
from tensorflow.python.pywrap_tensorflow_internal import *
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 28, in <module>
_pywrap_tensorflow_internal = swig_import_helper()
File "C:\Users\Hector Gonzalez\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.1.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 24, in swig_import_helper
_mod = imp.load_module('_pywrap_tensorflow_internal', fp, pathname, description)
File "imp.py", line 242, in load_module
File "imp.py", line 342, in load_dynamic
ImportError: DLL load failed: Error en una rutina de inicialización de biblioteca de vínculos dinámicos (DLL).
Failed to load the native TensorFlow runtime.
See https://www.tensorflow.org/install/errors
for some common reasons and solutions. Include the entire stack trace
above this error message when asking for help.
[13164] Failed to execute script stm32ai
2020-06-17 11:17 PM
Dont want to state the obvious but a seems like a DLL is missing. Can you please translate that import error?
2020-06-18 6:59 PM
Thanks for helping. import error translation is as follows::
A dynamic link library (DLL) initialization routine failed.
I have tried installing Visual C++ 2015-2019 as mention on some post.
2021-05-16 1:40 AM
Hi, have you found a workaround for this error in the end? I am also stuck at this but I didn't find anything else online. Thanks :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.