2025-08-25 12:12 AM
2025-08-25 1:19 AM
Hello @Kumar123,
You have the ST Model Zoo: GitHub - STMicroelectronics/stm32ai-modelzoo: AI Model Zoo for STM32 devices
That contains model that you can use with the ST Model Zoo Services or with the Standalone getting started
ST Model Zoo Services: GitHub - STMicroelectronics/stm32ai-modelzoo-services: AI Model Zoo services for STM32 devices
Standalone getting started: STM32N6-AI | Software - STMicroelectronics
With the ST Model Zoo Services, you can find documentation to retrain a model, quantize a model, evaluate a model, deploy a model etc. You need to edit the user_config.yaml and run the stm32_main.py script.
With the Standalone getting started, you can replace the default model with models from the model zoo. See the doc in /Doc (you will mainly need to convert the model to c and edit the postprocessing).
Have a good day,
Julian
2025-08-25 4:59 AM
Dear Julian
Thank you for your response. I’ve installed the packages, but I’m not familiar with the Model Zoo. I’ve chosen the image_classification example—how do I implement it? Please guide me step by step
GitHub - STMicroelectronics/stm32ai-modelzoo: AI Model Zoo for STM32 devices
GitHub - STMicroelectronics/stm32ai-modelzoo-services: AI Model Zoo services for STM32
STM32N6-AI | Software - STMicroelectronics
2025-08-25 8:14 AM
Hello @Kumar123,
For image classification, everything is explained in the different readme:
You will find a link for each operation modes (training, quantization, deployement ect) with step by step guide.
Keep in mind that the way it works is similar. It is always:
Have a good day,
Julian
2025-08-25 11:14 PM
Dear Julian
Why do we need to edit the user_config.yaml file? If we run the script directly without editing it, will it still work?
2025-08-26 12:49 AM
Hello @Kumar123,
You can edit the yaml to configure what you want to do:
Depending on what you do, you will also need to set your path to cubeIDE, ST Edge AI Core etc
Please read the documentation.
Have a good day,
Julian
2025-09-03 3:00 AM
Dear Julian
I run script getting errors in image classification example.
File "d:\Pavan\AI Software packages\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 11, in <module>
from hydra.core.hydra_config import HydraConfig
ModuleNotFoundError: No module named 'hydra'
PS D:\Pavan\AI Software packages\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification>
2025-09-04 7:51 AM - edited 2025-09-04 7:53 AM
Hello. Here is a helpful guide AI:How to use Teachable Machine to create an image classification application on STM32 - stm32mcu
Different board should not be a big problem. I guess you need the stage "3. Porting to a target".
Try to install correct python version(3.9 or 3.10) and correct requirements from requirements.txt.
2025-09-06 12:00 AM
Hi Avburmel
I think the next step is Stage 3: Porting to a target. How do I port to a target? I installed the ModelZoo services and the required packages. I tried the image classification example, but when I run stm32ai_main.py, I get errors. Please check.
PS D:\Micro\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification> & C:/Users/User/AppData/Local/Programs/Python/Python39/python.exe d:/Micro/stm32ai-modelzoo-services-main/stm32ai-modelzoo-services-main/image_classification/stm32ai_main.py
[INFO] : Setting upper limit of usable GPU memory to 24GBytes.
[INFO] : Running `chain_tqeb` operation mode
Error executing job with overrides: []
Traceback (most recent call last):
File "C:\Users\User\AppData\Local\Programs\Python\Python39\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "d:\Micro\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 374, in main
cfg = get_config(cfg)
File "d:\Micro\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification\src\utils\parse_config.py", line 327, in get_config
parse_dataset_section(cfg.dataset,
File "d:\Micro\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification\src\utils\parse_config.py", line 84, in parse_dataset_section
_check_dataset_paths_and_contents(cfg, mode=mode, mode_groups=mode_groups)
File "d:\Micro\stm32ai-modelzoo-services-main\stm32ai-modelzoo-services-main\image_classification\src\utils\parse_config.py", line 42, in _check_dataset_paths_and_contents
raise FileNotFoundError(f"\nUnable to find the root directory of the {name[:-5]} set\n"
FileNotFoundError:
Unable to find the root directory of the training set
Received path: ./datasets/flower_photos
Please check the 'dataset' section of your configuration file.
Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.
2025-09-08 2:08 AM - edited 2025-09-08 2:11 AM
Hi. I guess you need to download and unzip to "./datasets/flower_photos" flower_photos dataset to train your model.
https://storage.googleapis.com/download.tensorflow.org/example_images/flower_photos.tgz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.