2025-05-22 7:40 PM
Hello
I want to use ST Edge AI Core for model validate on STM32MP257.
When I set the parameter --mode host, the report results include "Inference time per node"
command: stedgeai validate -m ./linear_model_quantized.onnx --target stm32mp2 --mode host -v 2
part of report result:
Inference time per node
---------------------------------------------------------------------------
c_id m_id type dur (ms) % cumul name
---------------------------------------------------------------------------
0 0 NL (0x107) 0.001 30.8% 30.8% ai_node_0
1 18 Dense (0x104) 0.001 30.8% 61.5% ai_node_1
2 18 NL (0x107) 0.001 26.9% 88.5% ai_node_2
---------------------------------------------------------------------------
n/a n/a Inter-nodal 0.000 11.5% 100.0% n/a
---------------------------------------------------------------------------
total 0.003
---------------------------------------------------------------------------
But I want to see the actual inference time of each layer of the model running on NPU.
So, I run command: stedgeai validate -m ./linear_model_quantized.onnx --target stm32mp2 --mode target -d mpu:192.168.0.10:npu -v 2
report is in attach files,without infomation "Inference time per node"
Is it because the validation on STM32MP257 does not support "Inference time per node", or did I use incorrect tool parameters or firmware version?
Thanks
Solved! Go to Solution.
2025-05-23 6:03 AM
Hello @charlie128,
The validate mode is made to compare the generated NBG model and the original onnx model.
The goal is not to benchmark the model on the board.
To benchmark the model, you need to send it on the target and do a x-linux-ai-benchmark.
I am not sure that per layer inference time is a feature.
Learn more here:
https://wiki.st.com/stm32mpu/wiki/How_to_deploy_your_NN_model_on_STM32MPU
https://wiki.st.com/stm32mpu/wiki/How_to_benchmark_your_NN_model_on_STM32MPU
Have a good day,
Julian
2025-05-23 6:03 AM
Hello @charlie128,
The validate mode is made to compare the generated NBG model and the original onnx model.
The goal is not to benchmark the model on the board.
To benchmark the model, you need to send it on the target and do a x-linux-ai-benchmark.
I am not sure that per layer inference time is a feature.
Learn more here:
https://wiki.st.com/stm32mpu/wiki/How_to_deploy_your_NN_model_on_STM32MPU
https://wiki.st.com/stm32mpu/wiki/How_to_benchmark_your_NN_model_on_STM32MPU
Have a good day,
Julian
2025-05-24 7:19 PM
Thanks alot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.