2023-09-08 6:49 AM
Hello,
Has anyone worked with LSM303AGR sensor in Simulink. I am trying to interface the sensor and update values continously from board in simulink displays. I have been tryin to set up the connection for so long but nothing seems to be working and I am enable to establish a connection to the simulink model. could anyone experienced with STM32 embedded coder support package help me in making this work.
my equipment and software details are
USB TTL 232 RPi cable for serial communication
Board: STM32F411VET Discovery
MEMS accelerometer/Gyroscope: LSM303AGR via I2C1 @ PB6 and PB9
MATLAB 2023a and CubeMX
my last error was
"Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT command"
2023-09-08 6:55 AM
Hello @sanathhere
If you are just using simulink for display values . I suggest you to use LabVIEW wish is more easy to use and adapted to STM32 boards using an STM32 toolbox.
Best regards.
II
2023-09-08 6:59 AM
It not just to display values, I plan to further develop a model in simulink based on the accelerometer values and then further eastablish a motor control after my math model to automate a tilting mechanism for a 3 wheeled vehicle, accelerometer being my input amongst other things and output would be the automated motor control.
I wrote you a personal message in the hope you would know more about the interface and could help me, if you could spare some time would be very helpful
2023-09-08 7:10 AM - edited 2023-09-08 7:12 AM
I still advise you to use LabVIEW. It can do all the work you're planning to do it.
Best regards.
II
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.