2025-06-26 11:53 PM
Hello everyone,
I encountered an issue while using ST Edge AI 2.1.0 and I would appreciate some help.
Here is my original CUSTOM_MPOOLS configuration, which worked perfectly:
However, when I added the following options to the options section:
I received the following error:
I referred to the official documentation and saw that it does mention using these commands to modify the input/output requirements of the model. However, it seems that these commands are not fully supported in ST Edge AI 2.1.0, which is causing the error above.
My questions are:
Why does adding --input-data-type uint8 --inputs-ch-position chlast --output-data-type float32 cause this error?
Are these commands incompatible with ST Edge AI 2.1.0, or is there another configuration issue?
Is there another way to modify the input/output data formats, or are there specific things I need to be aware of?
Thank you in advance for your help!
Solved! Go to Solution.
2025-06-27 1:15 AM
Hello @qiqi,
These three option are front end option, meaning that they are used in the stedgeai command, not in the aton profiles.
Remove these from the profiles in user_neuralart.json and use them instead like this:
stedgeai.exe generate --model .... --target stm32n6 --st-neural-art --input-data-type ... --output-data-type ... --input-ch-position ...
Have a good day,
Julian
2025-06-27 1:15 AM
Hello @qiqi,
These three option are front end option, meaning that they are used in the stedgeai command, not in the aton profiles.
Remove these from the profiles in user_neuralart.json and use them instead like this:
stedgeai.exe generate --model .... --target stm32n6 --st-neural-art --input-data-type ... --output-data-type ... --input-ch-position ...
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.