2025-01-30 8:26 AM
Hello everyone,
I’m trying to run a model on an STM32 MCU with Neural-ART using the ST Edge AI Developer Cloud.
The final model includes GRU layers, but when I attempt to quantize and then optimize it, I encounter issues. To debug this, I created a minimal test model, which is as follows:
class GRUTEST(nn.Module):
def __init__(self, hidden_layer_size, n_layers, output_size, dropout, device):
super(GRUTEST, self).__init__()
self.device = device
self.hidden_layer_size = hidden_layer_size
self.n_layers = n_layers
self.rnn = nn.GRU(256, hidden_layer_size, n_layers, batch_first=True, dropout=dropout, bidirectional=False)
self.fc = nn.Linear(64, output_size)
def forward(self, x):
x, _ = self.rnn(x)
x = self.fc(x[:, -1, :])
return xI then convert this model to ONNX as follows:
torch_model = GRUTEST(
hidden_layer_size=64,
n_layers=2,
output_size=1,
dropout=0.2,
device='cpu'
)
torch_model.eval()
torch.onnx.export(
torch_model,
torch.randn(1, 1, 256),
"modelGRU.onnx",
opset_version=15,
input_names=["input"],
output_names=["output"],
dynamic_axes={"input": {0: "batch_size"}, "output": {0: "batch_size"}},
export_params=True,
keep_initializers_as_inputs=False
)I successfully perform per-channel quantization, but as soon as I reach the optimization step (with default optimization options), I get the following error—both with the quantized and non-quantized versions of the model:
TOOL ERROR: operands could not be broadcast together with shapes (256,) (128,).
If I replace the GRU with an LSTM model:
class LSTMTEST(nn.Module):
def __init__(self, hidden_layer_size, n_layers, output_size, dropout, device):
super(LSTMTEST, self).__init__()
self.device = device
self.hidden_layer_size = hidden_layer_size
self.n_layers = n_layers
self.rnn = nn.LSTM(256, hidden_layer_size, n_layers, batch_first=True, dropout=dropout, bidirectional=False)
self.fc = nn.Linear(64, output_size)
def forward(self, x):
batch_size = x.size(0)
h_0 = torch.zeros(self.n_layers, batch_size, self.hidden_layer_size, device=x.device)
c_0 = torch.zeros(self.n_layers, batch_size, self.hidden_layer_size, device=x.device)
x, _ = self.rnn(x, (h_0, c_0))
x = self.fc(x[:, -1, :])
return xEven though I explicitly define h_0 and c_0, I still get the following error:
NOT IMPLEMENTED: Sixth input (initial_h) of LSTM _rnn_LSTM_output_0_forward is not constant or constant propagation was not able to compute it
Would anyone be able to point out what I’m doing wrong?
Thanks in advance!
Solved! Go to Solution.
2025-01-31 6:59 AM
Hello @Dresult,
The neural-art does not support GRU nor LSTM. You can find the list of supported layers here:
https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_operator_support.html
Have a good day,
Julian
2025-01-31 6:59 AM
Hello @Dresult,
The neural-art does not support GRU nor LSTM. You can find the list of supported layers here:
https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_operator_support.html
Have a good day,
Julian
2025-02-03 3:27 AM
Hello @Julian E.
Thanks for your answer, I hadn't check the page dedicated to the NPU. Now, it makes sense.
However, I am also trying to deploy the model on the STM32 MCUs and MPUs but when it comes to the optimaztion step, the process hangs. I tried with both the ST Edge AI Core 2.0 and the STM32Cube.AI 9.0. Do GRU and LSTM layers remain unsupported even on these platforms ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.