2025-03-20 3:16 AM
Hello everyone,
I am trying to convert a tf.matmul operation into a .tflite model and deploy it on the STM32MP257F-EV1 NPU for acceleration. My inference inputs are (1, 1, 384) and (1, 51865, 384). Below is my code:
import tensorflow as tf
import numpy as np
hidden_states = tf.keras.Input(shape=(1, 384), dtype=tf.float32)
output_embeddings = tf.keras.Input(shape=(51865, 384), dtype=tf.float32)
output = tf.matmul(hidden_states, output_embeddings, transpose_b=True)
# Create a new standalone model
matmul_model = tf.keras.Model(inputs=[hidden_states, output_embeddings], outputs=output)
matmul_model.summary()
# Define the inputs
hidden_states = tf.random.normal((1, 1, 384), dtype=tf.float32) * 3
output_embeddings = tf.random.normal((1, 51865, 384), dtype=tf.float32) * 3
# Call the model with separate arguments
output = matmul_model([hidden_states, output_embeddings])
print(output.shape)
matmul_model.save("matmul_saved_model", save_format="tf")
# Load the saved encoder model
matmul_model = tf.keras.models.load_model("matmul_saved_model")
# Function to generate representative dataset
def representative_data_gen():
for _ in range(10): # 10 samples for calibration
hidden_states = np.random.normal(size=(1, 1, 384)).astype(np.float32)
output_embeddings = np.random.normal(size=(1, 51865, 384)).astype(np.float32)
yield [hidden_states, output_embeddings]
# Function to convert and quantize models to .tflite
def convert_and_quantize_to_tflite(model_path, output_tflite_path, representative_data_gen):
model = tf.keras.models.load_model(model_path)
converter = tf.lite.TFLiteConverter.from_keras_model(model)
# Enable post-training quantization
converter.optimizations = [tf.lite.Optimize.DEFAULT]
# Provide the representative dataset for proper scaling
converter.representative_dataset = representative_data_gen
converter._experimental_disable_per_channel = True
converter._experimental_new_quantizer = False
# Ensure we use 8-bit asymmetric quantization
converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]
# Keep input and output in float32 for compatibility
converter.inference_input_type = tf.float32
converter.inference_output_type = tf.float32
# Convert and save the TFLite model
tflite_model = converter.convert()
with open(output_tflite_path, "wb") as f:
f.write(tflite_model)
print(f"{output_tflite_path} saved successfully.")
# Convert the model with quantization
convert_and_quantize_to_tflite("matmul_saved_model", "matmul_int8.tflite", representative_data_gen)
Following the ST Edge AI tool guide, I used the command:
./stedgeai generate --target stm32mp25 -m matmul_int8.tflite --input-data-type float32 --output-data-type float32
However, I encountered the following error:
ST Edge AI Core v2.0.0-20049
PASS: 0%| | 0/2 [00:00<?, ?it/s]E 17:17:28 Acuity need 2 input files, but got 1
INTERNAL ERROR: ('Acuity need 2 input files, but got 1', None)
Does anyone know what might be causing this issue?
Is it possible to deploy a model with multiple inputs on the NPU?
Or am I missing something in my conversion process?
Any insights or suggestions would be greatly appreciated!
Thank you in advance for your help!
2025-04-08 2:51 AM
Hello @Justin_wu,
Sorry for the late answer, I had big troubles with my pc so I took me quite some time to test your issue out.
It seems that in your code:
hidden_states = tf.keras.Input(shape=(1, 384), dtype=tf.float32)
output_embeddings = tf.keras.Input(shape=(51865, 384), dtype=tf.float32)
output = tf.matmul(hidden_states, output_embeddings, transpose_b=True)
the transpose_b=true is not supported.
If you do a transpose to 'output_embeddings' and remove 'transpose_b', it works.
hidden_states = tf.keras.Input(shape=(1, 384), dtype=tf.float32)
output_embeddings = tf.keras.Input(shape=(384,51865), dtype=tf.float32)
output = tf.matmul(hidden_states, output_embeddings)
Have a good day,
Julian
2025-04-08 6:59 AM
Hello @Justin_wu,
Also, we find a bug thanks to your code, please avoid naming any of your input with "output".
It should be fixed, but for now, make sure not to use it.
Have a good day,
Julian
2025-04-11 11:15 PM
Hello Julian E.,
I appreciate your reply and clarification a lot! I follow your suggestion, change my code to the following:
hidden_states = tf.keras.layers.Input(shape=(1, 384), dtype=tf.float32)
output_embeddings = tf.keras.layers.Input(shape=(384, 51865), dtype=tf.float32)
result = tf.matmul(hidden_states, output_embeddings)
matmul_model = tf.keras.Model(inputs=[hidden_states, output_embeddings], outputs=result)
# Define the dummpy inputs
hidden_states = tf.random.normal((1, 1, 384), dtype=tf.float32)
output_embeddings = tf.random.normal((1, 384, 51865), dtype=tf.float32)
result = matmul_model([hidden_states, output_embeddings])
matmul_model.save(f"matmul_saved_model", save_format="tf")
def representative_data_gen():
for _ in range(10): # 100 samples for calibration
hidden_states = np.random.normal(size=(1, 1, 384)).astype(np.float32)
output_embeddings = np.random.normal(size=(1, 384, 51865)).astype(np.float32)
yield [hidden_states, output_embeddings]
# Function to convert and quantize models to .tflite
def convert_and_quantize_to_tflite(model_path, output_tflite_path, representative_data_gen):
model = tf.keras.models.load_model(model_path)
converter = tf.lite.TFLiteConverter.from_keras_model(model)
# Enable post-training quantization
converter.optimizations = [tf.lite.Optimize.DEFAULT]
# Provide the representative dataset for proper scaling
converter.representative_dataset = representative_data_gen
converter._experimental_disable_per_channel = True
converter._experimental_new_quantizer = False
# Ensure we use 8-bit asymmetric quantization
converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]
# Keep input and output in float32 for compatibility
converter.inference_input_type = tf.float32
converter.inference_output_type = tf.float32
# Convert and save the TFLite model
tflite_model = converter.convert()
with open(output_tflite_path, "wb") as f:
f.write(tflite_model)
print(f"{output_tflite_path} saved successfully.")
# Convert the model with quantization
convert_and_quantize_to_tflite(f"matmul_saved_model", f"matmul_int8.tflite", representative_data_gen)
But I still get the same error when I try to convert .tflite to .nb format by the code:
$ ./stedgeai generate --target stm32mp25 -m ./matmul_int8.tflite --input-data-type float32 --output-data-type float32
ST Edge AI Core v2.0.0-20049
PASS: 0%| | 0/2 [00:00<?, ?it/s]E 14:07:53 Acuity need 2 input files, but got 1
INTERNAL ERROR: ('Acuity need 2 input files, but got 1', None)
So I wonder whether the way I use to generate .tflite is wrong? Or do I use the wrong command when using ST Edge AI tool to convert .nb format? Thanks a lot!
Best regards,
Justin
2025-04-15 8:00 AM
Hello @Justin_wu,
I use:
I copied and executed your code to generate the .tflite and ran your exact command in a git bash terminal and it worked.
I attach the complete folder to this message.
You can look at /st_ai_output/network_generate_report.txt to have the output of my generate command.
Have a good day,
Julian
2025-04-19 3:37 AM
Hello Julian E.,
Thanks for you test again! But it's weird that I still have problems when try to convert the matmul_int8.tflite, even though I use the .tflite in you test_user.zip.
So I wonder whether I use the tool in a wrong way or didn't install correctly. I cannot find the files in the st_ai_ws repository inside your test_user.zip, even after I convert other .tflite models correctly to .nb, those files won't be generated.
Here's how I install and use the tools in detail:
I use stedgeai-linux-onlineinstaller in the en.stedgeai-lin.zip got from https://www.st.com/en/development-tools/stedgeai-core.html to install the ST Edge AI tool, and between the installing process, it ask me to provide st neural-art archive, so I upload the en.stedgeai-stneuralart-10.0.0.zip.
After finishing installation, I use command
./stedgeai generate --target stm32mp25 -m ./matmul_int8.tflite --input-data-type float32 --output-data-type float32
under the path ~/stedgeai_tool/2.0/Utilities/linux
When I convert some model, say, model1.tflite into model1.nb, it generates ./stm32ai_ws/report_mode1.json. It also generates mode1.nb and two empty folder /inc and /src under ./stm32ai_output.
May I ask you how you get the files under your ./stm32ai_ws and ./stm32ai_output inside the test_user.zip?
Maybe there is something wrong when I install the ST Edge AI tool? Thanks!
Sorry for bothering you again.
Best regards,
Justin
2025-04-22 7:07 AM
Hello @Justin_wu,
I made a mistake sorry, I did not use the stm32mp2 as a target.
Because mcu, mpu and npu are different, the supported layers are different and you can get different error.
The stedge ai core for MPU is supported only on linux. I need to find a pc with linux to test it out.
I'll update you as soon as possible.
Have a good day,
Julian
2025-04-24 2:47 AM
Hello @Justin_wu,
So the issue is that --input-data-type and --output-data-type are not supported for stm32mp
Without these argument, the model do not create errors with the stedgeaicore
have a good day,
Julian
2025-05-23 12:52 AM - edited 2025-05-23 12:54 AM
Hello @Justin_wu,
Thanks for your replies, it did succeed, but the accuracy drop seems too high to be acceptable.
Actually, when I tried to convert other .tflite models containing linear, convolution, or activation layers, if I didn't add --input-data-type float32 and --output-data-type float32, the converted .nb model suffered an unacceptable accuracy drop.
Therefore, I wonder whether the two arguments are effective for --target stm32mp2?
May I ask you the official have an SOP or guideline to generate .tflite model and convert to .nb? Because I have been curious about whether the way I used is the correct way to generate .tflite, like mobilenet_v2_1.0_224_int8_per_tensor.tflite in the official github https://github.com/STMicroelectronics/meta-st-x-linux-ai/tree/main/recipes-samples/image-classification/models/files
Thanks!
Best regards,
Justin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.