2020-03-25 3:31 AM
I am building CNN model on TensorFlow and after that I generate C code for STM32 micro using CubeMX-AI.
Here's my model
model = models.Sequential()
model.add(layers.Conv2D(32, (3, 3), activation='relu', input_shape=(32, 32,1)))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.Flatten())
model.add(layers.Dense(32, activation='relu'))
model.add(layers.Dense(4))I tested it on micro controller and get good results.
here's the result of the 4 classes when input belongs to 3rd class
Output =-9.430237
Output =-7.165620
Output =1.203057
Output =-10.133130
but in order to get the probability I added SoftMax classifier to the last layer, here's the new model
model = models.Sequential()
model.add(layers.Conv2D(32, (3, 3), activation='relu', input_shape=(32, 32,1)))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.Flatten())
model.add(layers.Dense(32, activation='relu'))
model.add(layers.Dense(4, activation='softmax'))
after testing the modified model, results are OK for 3 classes -1st,2nd and 4th class- but I get wrong results for the 3rd class.
here's the output of the 4 classes while using input of the 3rd class
Output =0.523477
Output =0.476523
Output =0.000000
Output =0.000000according to my understanding the SoftMax is just exp(out_i)/sum(exp(out_j)) and the results Should be
am I doing something wrong or do I understand SoftMax function mistakenly ?
or there's something wrong in my tensorflow model?
2020-03-25 8:31 AM
Hi HAlzo,
Your understanding of Softmax is correct and X-CUBE-AI implements it correctly normally. Can you indicate me how you have generated the results (with and w/o softmax)?
Is it a STM32 project through STM32CubeIDEI? Project is gcc-base?
Have you generated the project with the option: -mfloat-abi=soft?
br,
Jean-Michel
2020-03-26 5:04 AM
Hi jean,
I am using STM32H734, so my FPU options are "-mfloat-abi=hard -mfpu=fpv5-d16"
Yes my project is generated using STM32CubeMx Ver 5.6.0 with X-Cube-AI version 5.0.0
Yes Project is gcc base , I am using SW4STM32 IDE
When SoftMax is included in my .h5 model , I just Perform the inference with the input data and print the output data
res = aiRun(in_data/*object*/, out_data);
if (res) {
// ...
printf("Error %d",res);
return;
}
/* Post-Process - process the output buffer */
// ...
char buffer[32] = {0};
sprintf(buffer, "Output =%f \n", out_data[0]);
printf(buffer);
sprintf(buffer, "Output =%f \n", out_data[1]);
printf(buffer);
sprintf(buffer, "Output =%f \n", out_data[2]);
printf(buffer);
sprintf(buffer, "Output =%f \n", out_data[3]);
printf(buffer);and when soft max is not included in the model , I Perform the inference, then apply softmax in my code on the output and print the results
res = aiRun(in_data/*object*/, out_data);
if (res) {
// ...
printf("Error %d",res);
return;
}
/* Post-Process - process the output buffer */
// ...
char buffer[32] = {0};
ai_double softmax[4], sum, max_prob;
ai_i8 max_index = 0;
sum=0.0;
for (int i = 0;i<4;i++) //calculate exp of outputs
{
softmax[i] = exp(out_data[i]);
sum+= softmax[i];
}
for (int i = 0;i<4;i++) //Normalize the results
{
softmax[i] = softmax[i]/sum;
}
max_prob=0;
for (int i = 0;i<4;i++) //Find the max
{
if(softmax[i]>max_prob)
{
max_prob = softmax[i];
max_index = i;
}
}
printf( "pattern %d, with prob %f\n",max_index+1,max_prob);br,
Hossam Alzomor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.