cancel
Showing results for 
Search instead for 
Did you mean: 

Is Cube-AI based on ARM CMSIS-NN?

RKopp.12
Associate II

How Cube-AI is different from ARM CMSIS-NN and ARM NN SDK?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
jean-michel.d
ST Employee

​Hello,

Currently X-Cube-AI 3.3.0 provides only a support for the floating point model (float32). It provides its own STM32 optimized libraries (mainly based on a ARM Cortex-M with FPU single precision). ARM CMSIS-NN package is only for the fixed-point support (q8, q16) and to use the Cortex-M DSP/SIMD extensions. Future X-Cube-AI release will have a fixed-point support which will be based on the low-level ARM CMSIS-NN functions.

X-Cube-AI vs ARM-NN-SDK?

ARM-NN is actually only an inference engine for CPUs, GPUs and NPUs (ARM Cortex CPUs, ARM Mali GPU,...), it is currently not compatible with Cortex-M microcontrollers. There is not an official Cortex-M support through the ARM-NN-SDK (or derived) on the top of the CMSIS-NN library (model translator or convertor point of view) to generate an optimized C-model implementation.

Best Regards,

Jean-Michel  

Thanks Jean. Cheers!

What about Cube-AI vs CMSIS-NN from performance perspective? CMSIS NN claims 4x runtime improvement due to, as you've already said, fixed point calculations. On the other hand, their library support seems messy: you need manually add layer by layer in your source code. I'd like to see a simple comparison of memory and FPS for MNIST model with CubeAI and CMSIS NN backends.

Thank you.

Hi ST, Recently Google released experimental version of TensorFlow Lite for ARM micro controllers. Can we have ST AI framework integrated with CMSIS-NN as a backend and TF-Lite as a front end please? This will reduce the fragmentation of AI frameworks on micro controllers. Get Outlook for Android<>
JNord
Associate II

In X-CUBE-AI 4.0 there is support for quantized TensorFlow Lite / Keras. But will it use the actually use the SIMD instructions of an M4F if using 8-bit quantization (like CMSIS-NN)?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.