2019-12-24 11:12 AM
I am looking to create a project where I can set/latch the interrupt pin INT1 on high when the LSM6DSOX is detecting state X (where X is state 1/2/3 etc.) and goes down (low) when in a generic/static state (state 0). How is this possible? I found in one of the application notes that the PAGE_RW flag (17h) has something to do with the flag. However, I am not able to find how I can customize the output signal like described above.
Has anyone experience with interrupts and how should one do this?
Solved! Go to Solution.
2020-04-03 7:19 AM
Hi @TSchi.2269 , is this topic related to this thread? Regards
2020-04-03 7:19 AM
Hi @TSchi.2269 , is this topic related to this thread? Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.