2026-04-12 2:57 AM - last edited on 2026-04-13 4:44 AM by Andrew Neil
Hi all,
I’m currently working on an Edge AI project using the NUCLEO-N657X0-q and I've run into a roadblock regarding multi-model deployment.
I need to run 2 or 3 models on this MCU, scheduled via FreeRTOS. While I can get a single model working fine with STM32Cube.AI Studio, I’m struggling to find a detailed workflow for managing multiple instances.
Specific questions:
API Naming: How to properly configure Cube.AI to generate unique prefixes for multiple models to avoid link-time conflicts?
Memory/Buffer Sharing: Is there a standard way to share a single activation buffer between models to save RAM, given they are called sequentially via FreeRTOS?
Task Scheduling: Any known issues or best practices for calling stai_network_run() within a FreeRTOS task? (e.g. stack size or re-entrancy).
I’ve checked the ST Edge AI Core docs but couldn't find a concrete example for this multi-model + RTOS use case. If anyone has a reference project or can point me to the right Application Note, I’d really appreciate it.
Thanks!
Solved! Go to Solution.
2026-04-13 4:30 AM
Hello @Jason32
When working with multiple networks / multiple instances, you need to specify a "model name".
ST Edge AI Core API uses stai_<network_name>_run() methods, which can be specified in STM32Cube AI Studio.
In the "Right Panel", scroll to "Advanced Settings" and in "Common Options", edit "network" by a string which is friendly to you (example: img_detect_1).
All the code generated (sources and headers) will be with this name:
network.c -> img_detect_1.c
network_data.c -> img_detect_1_data.c
etc...
To share a single activation buffer, allocation needs to be the greater one. If you are working with a contiguous memory region, and working with 3 models, you need to allocate a memory region which is the maximum of the 3.
Best regards,
Yanis
2026-04-13 4:30 AM
Hello @Jason32
When working with multiple networks / multiple instances, you need to specify a "model name".
ST Edge AI Core API uses stai_<network_name>_run() methods, which can be specified in STM32Cube AI Studio.
In the "Right Panel", scroll to "Advanced Settings" and in "Common Options", edit "network" by a string which is friendly to you (example: img_detect_1).
All the code generated (sources and headers) will be with this name:
network.c -> img_detect_1.c
network_data.c -> img_detect_1_data.c
etc...
To share a single activation buffer, allocation needs to be the greater one. If you are working with a contiguous memory region, and working with 3 models, you need to allocate a memory region which is the maximum of the 3.
Best regards,
Yanis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.