2025-03-01 6:39 AM - last edited on 2025-03-01 7:10 AM by Andrew Neil
HI!
I am newbie to CUBE AI.
I m working on implementing my CNN network that takes input image of 128,128,1 (greyscale) and give an output of 3 classes {class1,class2,class3}.
i did convert and try my model to TFLITE successfully on python.
then i went to stmcube and did put the model using X-CUBE-AI application template .
my problem is with
int acquire_and_process_data(ai_i8* data[])
{
/* fill the inputs of the c-model
for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++ )
{
data[idx] = ....
}
*/
return 0;
}
my input buffer is like this
#define AI_NETWORK_IN_1_FORMAT (AI_BUFFER_FORMAT_FLOAT)
#define AI_NETWORK_IN_1_HEIGHT (128)
#define AI_NETWORK_IN_1_WIDTH (128)
#define AI_NETWORK_IN_1_CHANNEL (1)
#define AI_NETWORK_IN_1_SIZE (16384)
#define AI_NETWORK_IN_1_SIZE_BYTES (65536)
i tried putting image as image [128*128] and image[128][128]
Solved! Go to Solution.
2025-03-03 8:44 AM
Hello @YahiaHedna ,
you are using float input, please try to change the
int acquire_and_process_data(ai_i8* data[])
to
int acquire_and_process_data(ai_float* data[])
then pass a float array of size 128x128=16384 to data[idx]
Have a good day,
Julian
2025-03-03 8:44 AM
Hello @YahiaHedna ,
you are using float input, please try to change the
int acquire_and_process_data(ai_i8* data[])
to
int acquire_and_process_data(ai_float* data[])
then pass a float array of size 128x128=16384 to data[idx]
Have a good day,
Julian
2025-03-06 10:24 AM
Thank you Julian!
I figured out the problem and I was getting that error because of the improper data passing to the input layer.
Thanks again for your time!
2025-06-25 1:31 AM
1. My image data is transmitted through a serial port or USB. How can I convert this image data into the data that needs to be received by int acquire_ and_decess_data (ai_i8 * data [])?
2. Do I need to convert these image data into BMP format first, and then put it into ai_i8 * data []? However, this parameter does not provide array length data, nor do I have input parameters for length and width dimensions. How can I convert an image data into ai_i8 * data [] format?
2025-06-26 2:08 AM
Use netron to check the input type of your model, if its float, uint .....
Then, do change data from ai_i8 to your input type.
Finnally, if your input is 64x64, ur data should have 4096 values, that you pass to your ai_run
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.