2025-09-25 1:08 PM
Hi,
I would like to check if there is any one who could guide me through the jungle of using TFLM in my software. It seems that it don't matter what I do when building a TFLM as a static library and link it to my simple test program. I have tried a lot of configurations and a lot of tries to 16 byte align the model and arena for this, but I am still getting a hard fault because of unaligned access in the AllocateTensors call.
My align of the model looks like this:
alignas(16) const unsigned char g_model_data[] = ...and my code using TFLM looks as follows:
#include <cstring>
//#include "tensorflow/lite/micro/micro_op_resolver.h"
#include "tensorflow/lite/micro/micro_mutable_op_resolver.h"
//#include "tensorflow/lite/micro/kernels/micro_ops.h"
//#include "tensorflow/lite/micro/micro_log.h"
//#include "tensorflow/lite/micro/micro_error_reporter.h"
#include "tensorflow/lite/micro/micro_interpreter.h"
#include "tensorflow/lite/schema/schema_generated.h"
#include "tensorflow/lite/micro/system_setup.h"
#include "crack_model_quant.h"
#include "test_signals.h"
#include "TFRunner.h"
static inline bool is_aligned(const void* p, size_t n) {
return (reinterpret_cast<uintptr_t>(p) & (n - 1)) == 0;
}
// Round a pointer up to the next N-byte boundary (N must be power of 2)
template <size_t N>
static inline uint8_t* align_ptr(uint8_t* p) {
return reinterpret_cast<uint8_t*>(
(reinterpret_cast<uintptr_t>(p) + (N - 1)) & ~static_cast<uintptr_t>(N - 1));
}
// If you can’t regenerate easily, you can point to the next aligned address:
// const unsigned char* g_model = reinterpret_cast<const unsigned char*>(align_ptr<16>(const_cast<uint8_t*>(g_model_data)));
// const int g_model_len = g_model_data_len - (g_model - g_model_data);
// const unsigned char* g_model = g_model_data;
// const int g_model_len = g_model_data_len;
// Globals, used for compatibility with Arduino-style sketches.
namespace {
const tflite::Model* model = nullptr;
tflite::MicroInterpreter* interpreter = nullptr;
//static tflite::MicroErrorReporter micro_error_reporter;
int inference_count = 0;
//double scale = 0.032983943819999695;
//int zero_point = -1;
// float qScale = 0.032983943819999695;
// int8_t qZero = -1;
// constexpr int kTensorArenaSize = 100 * 1024;
// uint8_t tensor_arena[kTensorArenaSize];
// Choose a size that fits your model; increase if you see kTfLiteArenaRw overflow
constexpr size_t kArenaSize = 70 * 1024;
// Over-allocate and then align the working pointer to 16 bytes
// #if defined(__GNUC__)
// __attribute__((aligned(16)))
// #endif
alignas(16) static uint8_t g_arena_raw[kArenaSize + 16];
static uint8_t* g_arena = align_ptr<16>(g_arena_raw);
static size_t g_arena_len = kArenaSize; // keep logical size the same
} // namespace
TfLiteTensor* input = nullptr;
TfLiteTensor* output = nullptr;
float in_scale;
int in_zero;
int TFRunner::run()
{
// Enable the DBGMCU clock
__HAL_RCC_DBGMCU_CLK_ENABLE();
// Enable the debugger during Sleep mode
HAL_DBGMCU_EnableDBGSleepMode();
// Enable the debugger during Stop mode
HAL_DBGMCU_EnableDBGStopMode();
// Enable the debugger during Standby mode
HAL_DBGMCU_EnableDBGStandbyMode();
alignas(16) static uint8_t g_model_aligned[g_model_data_len];
memcpy(g_model_aligned, g_model_data, g_model_data_len);
const unsigned char* g_model = g_model_aligned;
const int g_model_len = g_model_data_len;
// Your code here
tflite::InitializeTarget();
// Map the model into a usable data structure. This doesn't involve any
// copying or parsing, it's a very lightweight operation.
model = tflite::GetModel(g_model);
if (model->version() != TFLITE_SCHEMA_VERSION) {
MicroPrintf(
"Model provided is schema version %d not equal "
"to supported version %d.",
model->version(), TFLITE_SCHEMA_VERSION);
return -1;
}
// This pulls in all the operation implementations we need.
// NOLINTNEXTLINE(runtime-global-variables)
static tflite::MicroMutableOpResolver<11> resolver;
// Pull in only the operation implementations we need.
// This relies on a complete list of all the ops needed by this graph.
// An easier approach is to just use the AllOpsResolver, but this will
// incur some penalty in code space for op implementations that are not
// needed by this graph.
//
// static tflite::AllOpsResolver resolver;
// NOLINTNEXTLINE(runtime-global-variables)
if (resolver.AddConv2D() != kTfLiteOk) {
return -1;
}
if (resolver.AddMaxPool2D() != kTfLiteOk) {
return -1;
}
if (resolver.AddFullyConnected() != kTfLiteOk) {
return -1;
}
if (resolver.AddSoftmax() != kTfLiteOk) {
return -1;
}
if (resolver.AddReshape() != kTfLiteOk) {
return -1;
}
if (resolver.AddExpandDims() != kTfLiteOk) {
return -1;
}
// if (resolver.AddQuantize() != kTfLiteOk) {
// return -1;
// }
// if (resolver.AddDequantize() != kTfLiteOk) {
// return -1;
// }
// if (resolver.AddMul() != kTfLiteOk) {
// return -1;
// }
// if (resolver.AddAdd() != kTfLiteOk) {
// return -1;
// }
// if (resolver.AddLogistic() != kTfLiteOk) {
// return -1;
// }
// Build an interpreter to run the model with.
static tflite::MicroInterpreter static_interpreter(
model, resolver, g_arena, g_arena_len);
interpreter = &static_interpreter;
// Sanity: the model must be 16B aligned (TFLM will then keep alignment for sub-allocs)
if (!is_aligned(g_model, 16)) {
MicroPrintf("Model not 16B aligned -> will likely hard fault");
return -2;
}
// Sanity: the arena base must be 16B aligned (TFLM will then keep alignment for sub-allocs)
if (!is_aligned(g_arena, 16)) {
MicroPrintf("Arena not 16B aligned -> will likely hard fault");
return -2;
}
// Allocate memory from the tensor_arena for the model's tensors.
TfLiteStatus allocate_status = interpreter->AllocateTensors();
if (allocate_status != kTfLiteOk) {
MicroPrintf("AllocateTensors() failed");
return -1;
}
// Obtain pointers to the model's input and output tensors.
input = interpreter->input(0);
output = interpreter->output(0);
in_scale = input->params.scale;
in_zero = input->params.zero_point;
// const float out_scale = output->params.scale;
// const int out_zero = output->params.zero_point;
// Keep track of how many inferences we have performed.
inference_count = 0;
MicroPrintf("Input dims %d", input->dims->size);
MicroPrintf("Output dims %d\n", output->dims->size);
MicroPrintf("Input type %d", input->type);
MicroPrintf("Output type %d", output->type);
// Do an inference for every value in test array
for (int8_t r = 0; r < (std::int8_t)TEST_SIGNALS_ROWS; r++)
{
for (int c = 0; c < (int)TEST_SIGNALS_COLS - 1; c++) {
//int8_t quantized_value = static_cast<int8_t>(TEST_SIGNALS_INT8[r][c] / in_scale) + qZero;
input->data.int8[c] = quantizeValue(TEST_SIGNALS[r][c]);
//input->data.f[c] = TEST_SIGNALS_INT8[r][c];
}
// Run the model on the data input and make sure it succeeds.
TfLiteStatus invoke_status = interpreter->Invoke();
if (invoke_status != kTfLiteOk) {
MicroPrintf("Invoke failed");
return -1;
}
auto should_be = (int8_t)TEST_SIGNALS[r][1000];
MicroPrintf("Result should be: %d", should_be);
for (int8_t x = 0; x < 3; x++)
MicroPrintf("Result %d is %d", x, static_cast<int8_t>(output->data.int8[x]));
MicroPrintf("\n\n");
}
return 0;
}
int8_t TFRunner::quantizeValue(float_t value)
{
int result = static_cast<int8_t>((value / in_scale) + in_zero);
if (result > 127) result = 127;
if (result < -128) result = -128;
return result;
}
extern "C" void* TFRunner_init()
{
return new TFRunner();
}
extern "C" int TFRunner_run(void* ptr)
{
TFRunner* instance = static_cast<TFRunner*>(ptr);
return instance->run();
}Some ideas around this would be really appreciated.
The fault looks like this:
HardFault!
HFSR: 0x40000000
CFSR: 0x01000000
MMFAR: 0x7E265275
BFAR: 0x7E265275
Solved! Go to Solution.
2025-09-30 2:53 AM
Hello @nilssonm,
Is this really a TFLM problem? I think it is a compiling problem or something like that because I have tried to disable the aligning check and this makes the problem disappear, but I realize that this is not the way to solve it.
> As I said, I don't know. You may have better luck on a TFLM forum...
If it is really TFLM that interest you, we can't help you. But if your point is to compare MCU vs NPU performance, you can use the ST Edge AI Core on the N6 to run a model only on the MCU and compare it to it running on NPU.
We have multiple script to help you with that.
CM55 validation: STM32N6 Example projects & tips for creating new projects
NPU validation: Getting started - How to evaluate a model on STM32N6 board
Have a good day,
Julian
2025-09-30 1:36 AM
Hello @nilssonm,
Sorry to hear that you're stuck.
On our side, we don't support TFLM, and I don't have any knowledge about it, so I cannot help you.
hopefully, some other community member will help you.
I can only ask you if there is any particular reason for you to use TFLM?
In case you are not aware, we provide a solution to use AI model on STM32 called ST Edge AI Core.
It could also enable you to use the acceleration offered by the NPU on the STM32N6 (as you tagged it) for int8 operations.
ST Edge AI Core doc:
https://stedgeai-dc.st.com/assets/embedded-docs/index.html
Have a good day,
Julian
2025-09-30 1:53 AM
Hello,
I am currently working on a thesis project and would like to compare the bare naked TFLM with no acceleration at all with the one you are mentioning using the NPU on the STM32N6.
Is this really a TFLM problem? I think it is a compiling problem or something like that because I have tried to disable the aligning check and this makes the problem disappear, but I realize that this is not the way to solve it.
The best,
Mats
2025-09-30 2:53 AM
Hello @nilssonm,
Is this really a TFLM problem? I think it is a compiling problem or something like that because I have tried to disable the aligning check and this makes the problem disappear, but I realize that this is not the way to solve it.
> As I said, I don't know. You may have better luck on a TFLM forum...
If it is really TFLM that interest you, we can't help you. But if your point is to compare MCU vs NPU performance, you can use the ST Edge AI Core on the N6 to run a model only on the MCU and compare it to it running on NPU.
We have multiple script to help you with that.
CM55 validation: STM32N6 Example projects & tips for creating new projects
NPU validation: Getting started - How to evaluate a model on STM32N6 board
Have a good day,
Julian
2025-09-30 3:19 AM
Ok, this maybe a way for me to do the evaluation. My target is to compare whether there is a big difference between using hardware acceleration in both speed and energy aspects.
I will check the links you provided for me and maybe I can reach out here in this forum again if I stumble on some problems with this. It sure seems a little bit advanced comparing to what I have been working with before, but still very interesting and fun.
The best,
Mats
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.