2021-11-29 6:13 AM
Did you ever prepare a guideline like this one https://wiki.st.com/stm32mcu/wiki/AI:How_to_perform_motion_sensing_on_STM32L4_IoTnode but for ASC instead?
I have my own two-classes NN, keras model and the B-L475E-IOT01.
After replacing asc and asc_data files in the FP-AI-SENSING1 package, building failed with errors and warnings that mostly are not related to the different inferences.
New ASC files are generated by the latest X-CUBE-AI and X-CUBE-MX but seem to be not compatible with the ones in FP-AI-SENSING1
Thanks
M
2021-12-14 3:56 AM
Hi,
When you do with your own dataset for ASC, use the below versions while creating neural networks models.
Keras---2.2.4
Tensor flow---1.14.0
Librosa---0.8.0
when you generate code in MX use below version.
STM32MX CUBE- 5.0
X-CUBE AI-4.1.0
Because, all codes in FP-AI-SENSING1 Pack, they have generated the code as mentioned above.
Regards,
shankari
2022-10-29 2:42 AM
As you commented, we need to use X-CUBE AI-4.1.0 to convert the network model for ASC to C source code. Otherwise, the source will not compile.
I wonder if there is a version of FP-AI-SENSING1 available for us to use CUBE AI 7.3.0 instead of CUBE AI-4.10.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.