2019-02-06 6:45 AM
I am following this video this, i have successfully generated the code, validate it on desktop, build the code and flash using Truestudio it into STM32L476RB board. But when I try to validate it om my board it gives me
error : board not found or invalid firmware or restart the board
I have also tried using different USART port, but no success.
I have aslo flash the code using CubeProgrammer. but still same error on validating.
CubeMX is able locate the port on which board is present but gives same error
2019-02-07 12:52 AM
Hello,
What OS are you using ?
Have you flash flash on target the right project (the Validation project) ?
What you can try is to connect to the STM32 via an serial terminal like Putty/Termite/TeraTerm... and see if you have some outputs
Be careful to disconnect the serial port before using CubeMX otherwise CubeMX will not be able to connect
Regards,
Romain
2019-02-07 3:42 AM
STM32L476RB is not a board name, it is a microcontroller. Find the exact name of your board.
-- pa
2019-02-08 2:07 AM
Thanks Everyone, There was problem in my compiler. Code isnow successfully validated. My board is Nucleo -L476RG.
2019-09-20 5:56 AM
Could you please tell me how you resolved this problem. I face the same problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.