2023-08-02 7:59 AM
Hello I have STEVAL-STWINKT1B device. When i try to connect wifi with tera term it gives this error:
platform_init L#234 The network interface can not be started
any advice?
2023-08-03 3:29 AM
Hi @bcryhun ,
it may depend on the firmware installed on the STWIN. can you check which is it?
this is the first I would try to work with WiFi: FP-AI-PREDMNT2
If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community
Niccolò
2023-08-06 3:50 AM - edited 2023-08-06 3:52 AM
i did use fp-ai-predmnt2 and follow steps on documentation. It is same, i can not connect to wifi. When i try to write ssid and password, it does not give any response
2023-08-07 12:53 AM
Hi @bcryhun ,
what toolchain did you use?
were you able to check with debug if the fw has some problem somewhere?
if you tell me where it gets stuck I can try to help you overcoming this issue =)
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.