2025-03-12 3:12 AM
Could Anyone please help me with the Example application where MDK-ARM toolchain is used to build the application using ST Neural-ART accelerator™. I have STM32N6570-DK evolution kit and I'm trying to develop a prototype for KWS usecase. We have already used the example project provided for STM32CubeIDE with GCC compiler to get started. But, there are no .IOC file is available to modify the example code to develop other use cases.
Also wanted to know, what if I build the application that uses ST-Neural-ART accelerator with MDK-ARM would it be able to take advantage of Arm compilor, or such applications can only build with STM32CubeIDE. If it can be build with MDK-ARM, Please provide the example reference so we can finalize the chip for our production.
2025-03-17 3:54 AM
Hello @Vishal95 ,
Sorry for the late answer.
As of today, we don't provide the .ioc (I don't know the exact reason).
You are not the only one to ask, so I transmitted the demand to the dev team.
As for your second question, there is no requierement to use STM32CubeIDE, the application can be compiled with IAR, GCC, ARM MDK etc..
We are working on an example with keil, but it is not a priority for the dev team. So, it will come, but I don't know when
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.