2019-10-03 7:36 AM
Hi experts!
I am trying to use a NN made on Keras on my NUCLEO-F303K8 (MCU STM32F303K8T6).
I've already configured my project, setup the USART2 and imported my NN (.h5)
I successfully validated my project on desktop but when I tried to validate it on target, I got:
ERROR: no connected board(s) or invalid firmware or the board should be re-started
I've updated all the firmwares and then tried to perform the validation with manual config (set USART2 with the right bound rate, SW4STM32, etc). And then now I am getting:
No board connected to the machine with MCU STM32F303K8TX
But this is exactly what my MCU is.
My versions:
STM32CubeMX - 5.2.0
Firmware - STM32Cube FW_F3 V1.10.0
X-CUBE-AI - 4.0.0
Eclipse - Neon.3 Release (4.6.3)
System Workbench for STM32 - Ac6 - 2.5.0.201904120827
I've also tried some solutions on other topics in the forum. None of them worked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.