2024-09-11 12:34 AM
Hello everyone,
I am learning how to use the ST Edge AI Developer Cloud tool and, after downloading my model that I developed with TensorFlow and selecting the STM32 MCUs platform, I wanted to try the post-training quantization but I encountered the following error:
Executing with: {'model': '/tmp/quantization-service/970d7e77-a0e3-4d23-a8ec-5e7e52d9a260/1dcnnrnn_01.h5', 'data': '/tmp/quantization-service/970d7e77-a0e3-4d23-a8ec-5e7e52d9a260/dataset4quantization.npz', 'input_type': tf.float32, 'output_type': tf.float32, 'optimization': <Optimize.DEFAULT: 'DEFAULT'>, 'output': '/tmp/quantization-service/970d7e77-a0e3-4d23-a8ec-5e7e52d9a260', 'disable_per_channel': False} Error when deserializing class 'InputLayer' using config={'batch_shape': [None, 9999, 1], 'dtype': 'float32', 'sparse': False, 'name': 'input_layer_4'}. Exception encountered: Unrecognized keyword arguments: ['batch_shape']
The error occurs regardless of weather I provide a data set for quantization or not.
Can anyone help me understanding what I have to change? Thank you in advance :)
Solved! Go to Solution.
2024-09-12 12:57 AM
Hello,
It means you are using operators that are not supported by the quantizer. Actually we only support
2024-09-11 4:32 AM
Hello,
Could you please tell me what is the version of Tensorflow used to export your model ?
I would first suggest to try using version 2.15 since it it the one used for quantization.
Best regards,
Yanis
2024-09-11 7:43 AM
Hello Yanis,
I used the version 2.17 to train and export the model. I downgraded to the 2.15 version to try to export again the model and load it in ST Edge AI Developer Cloud, but during the loading of the model in python I obtained the same error that I was encountering in the ST Edge AI Developer Cloud:
Error when deserializing class 'InputLayer' using config={'batch_shape': [None, 9999, 1], 'dtype': 'float32', 'sparse': False, 'name': 'input_layer_4'}. Exception encountered: Unrecognized keyword arguments: ['batch_shape']).
Do you have any suggestions? Should I retrain the network using the Tensorflow 2.15?
Best regards,
Silvia
2024-09-11 8:12 AM
Hello Silvia,
Yes, I would first suggest to retrain the network using TF 2.15, and see if the same issue occurs
Best regards,
Yanis
2024-09-12 12:42 AM
Thanks @hamitiya and @Destini.
I have retrained the model using the 2.15 version and, when I launched the quantization, that error didn't occur again.
But now I am encountering the following error, linked to some troubles that the converter has with some operations (TensorListReserve and StatefulPartitionedCall). How can I solve this issue? Is it possible to Select TF ops and disabling `_experimental_lower_tensor_list_ops` flag in the TFLite converter object - as suggested in the error window - directly using the ST Edge Ai Developer Cloud or do I have to implement the conversion to TFLite directly by myself in my python script?
Executing with: {'model': '/tmp/quantization-service/603561c5-0a56-4eee-b3dc-a1ee6ad23869/1dcnnrnn_00.h5', 'data': None, 'input_type': tf.float32, 'output_type': tf.float32, 'optimization': <Optimize.DEFAULT: 'DEFAULT'>, 'output': '/tmp/quantization-service/603561c5-0a56-4eee-b3dc-a1ee6ad23869', 'disable_per_channel': False} No data specified, enabling fake quantization Converting original model to TFLite... /app/quantizer/cli.py:53:1: error: 'tf.TensorListReserve' op requires element_shape to be static during TF Lite transformation pass res = quantize_from_local_file( ^ <unknown>:0: note: loc(fused["StatefulPartitionedCall:", "StatefulPartitionedCall"]): called from /app/quantizer/cli.py:53:1: error: failed to legalize operation 'tf.TensorListReserve' that was explicitly marked illegal res = quantize_from_local_file( ^ <unknown>:0: note: loc(fused["StatefulPartitionedCall:", "StatefulPartitionedCall"]): called from <unknown>:0: error: Lowering tensor list ops is failed. Please consider using Select TF ops and disabling `_experimental_lower_tensor_list_ops` flag in the TFLite converter object. For example, converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS, tf.lite.OpsSet.SELECT_TF_OPS]\n converter._experimental_lower_tensor_list_ops = False
Thanks for the help!
Best,
Silvia
2024-09-12 12:57 AM
Hello,
It means you are using operators that are not supported by the quantizer. Actually we only support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.