2025-06-18 6:49 AM
Hello,
I'm interested in understanding how much an NPU can accelerate a model. I reviewed the documentation for Neural Art and found that 38 TFLite operators are supported by the hardware:
ABS, ADD, AVERAGE_POOL_2D, BATCH_MATMUL, CAST, CEIL, CONCATENATION, CONV_2D, DEPTHWISE_CONV_2D, EQUAL, EXPAND_DIMS, FULLY_CONNECTED, HARD_SWISH, LEAKY_RELU, LOGICAL_AND, LOGICAL_NOT, LOGICAL_OR, LOGISTIC, MAX_POOL_2D, MUL, PACK, PAD, PRELU, (RE)QUANTIZE, RELU, RELU6, RESHAPE, RESIZE_NEAREST_NEIGHBOR (with coordinate_transformation_mode=asymmetric and nearest_mode=floor), SPACE_TO_DEPTH (with same input/output quantization), SPLIT, SPLIT_V, STRIDED_SLICE, SQUEEZE, SUB, TANH, TRANSPOSE, TRANSPOSE_CONV, UNPACK.
However, each operator has a different level of computational complexity. Therefore, the acceleration ratio provided by the NPU may vary depending on which operators are used. For example, a model that heavily uses CONV layers may benefit more from NPU acceleration than one that primarily uses ADD operations.
Do you have any documentation or benchmarks that show the computational intensity or NPU acceleration ratio for each of these supported operators, compared to running them on the CPU?
Solved! Go to Solution.
2025-06-25 2:31 AM - edited 2025-06-25 2:32 AM
Hello @Einstein_rookie_version,
We don't have such benchmark as a layer is not mapped one for one on an epoch.
The only benchmarks I can redirect you are the benchmarks of models from model zoo, for example:
In the tables you will find inference times for multiple models and boards. There is no direct comparison between n6 with and without the npu being used.
You also have the validate on target command with the st edge ai core to do your own benchmark:
https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_getting_started.html
Have a good day,
Julian
2025-06-25 2:31 AM - edited 2025-06-25 2:32 AM
Hello @Einstein_rookie_version,
We don't have such benchmark as a layer is not mapped one for one on an epoch.
The only benchmarks I can redirect you are the benchmarks of models from model zoo, for example:
In the tables you will find inference times for multiple models and boards. There is no direct comparison between n6 with and without the npu being used.
You also have the validate on target command with the st edge ai core to do your own benchmark:
https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_getting_started.html
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.