2026-04-10 6:12 AM
Yesterday I built a model from a 256x256x3 .tflite. The Cloud produced a zip file that included a network_atonbuf.xSPI2.raw file. This file is about 27KB in size.
What triggered the change from the network_data files?
The network.c knew about this .raw file and pointed at it 0x71000000. That's all good. I just rename it to .bin and loadi it with CubeProgrammer. But what I don't understand is the test for version:
#if LL_ATON_VERSION_MAJOR != 1 || LL_ATON_VERSION_MINOR != 1 || LL_ATON_VERSION_MICRO != 3 || LL_ATON_VERSION_DEV != 262
# error "Possible mismatch in ll_aton library used"
#endifWorking with the STM32N6-GettingStarted-ObjectDetection as my base this version test failed in Make. I just commented it out.
Am I going to have a problem?
Solved! Go to Solution.
2026-04-10 6:25 AM - edited 2026-04-10 6:30 AM
Hello @Duckpaddle
By default, when using ST Neural-ART, weights are produced as "raw" (binary) files instead of .c files. They need to be loaded via STM32CubeProgrammer at the specified address (here, 0x7100_0000).
In order to change this behavior, you can do it by editing the memory pools description:
- in C:\ST\STEdgeAI\4.0\Utilities\windows\targets\stm32\resources\NPU\STM32N6xx
- For XSPI2, replace FORMAT_RAW with FORMAT_C
Code you are refering to is in order to prevent mismatch between Neural-ART Library in your project and the one used to generate the code.
If you have mismatch, it means you used a different version of ST Edge AI Core.
LL_ATON 1.1.3.262 refers to ST Edge AI Core 4.0.0-20500 (latest available)
Best regards,
Yanis
2026-04-10 6:25 AM - edited 2026-04-10 6:30 AM
Hello @Duckpaddle
By default, when using ST Neural-ART, weights are produced as "raw" (binary) files instead of .c files. They need to be loaded via STM32CubeProgrammer at the specified address (here, 0x7100_0000).
In order to change this behavior, you can do it by editing the memory pools description:
- in C:\ST\STEdgeAI\4.0\Utilities\windows\targets\stm32\resources\NPU\STM32N6xx
- For XSPI2, replace FORMAT_RAW with FORMAT_C
Code you are refering to is in order to prevent mismatch between Neural-ART Library in your project and the one used to generate the code.
If you have mismatch, it means you used a different version of ST Edge AI Core.
LL_ATON 1.1.3.262 refers to ST Edge AI Core 4.0.0-20500 (latest available)
Best regards,
Yanis
2026-04-10 7:28 AM
For the other people that might have this issue and me after I forget,
I removed the comment block around the version test in network.c
I deleted the ./Middlewares/stedgeai-lib/Npu, then I copied my new ST Cloud subdirectory into the Npu subdirectory under ./Middlewares/stedgeai-lib/Npu
After a clean and make it worked great.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.