2026-03-03 5:22 AM
Dear all,
I am currently deploying the image_classification application.
So, from stm32ai-modelzoo-services (in my case, it is in the directory stm32ai-modelzoo-services4), I am using the following command with my configuration file:
python .\stm32ai_main.py --config-path . --config-name .\user_deployment_n6_config.yaml
I added some code in /common/stm32ai_local/build.py to help diagnose the programming of the STM32N6570-DK board.
The programming process seems to complete correctly, but when I restart the kit (with BOOT0 and BOOT1 set to the left), the screen remains black.
However, if I launch STM32CubeIDE, import my application, perform a build, and then a Run As, the programming works correctly and the application runs perfectly.
I believe the original goal is, of course, to be able to program and run my application directly using the script:
python .\stm32ai_main.py --config-path . --config-name .\user_deployment_n6_config.yaml
Please find attached the execution log of the script.
Many thanks in advance for your help.
Emmanuel
Solved! Go to Solution.
2026-03-04 4:14 AM
Dear all,
the solution is here : https://community.st.com/t5/edge-ai/a-bug-with-stm32cube-ide-2-0-0-and-stm32ai-modelzoo-services/td-p/883573
Cheers
Emmanuel
2026-03-03 8:19 AM
2026-03-03 11:58 AM
Hi,
I keep trying to make progress…
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection
in the documentation :
On STM32N6570-DK:
export DKEL="<STM32CubeProgrammer_N6 Install Folder>/bin/ExternalLoader/MX66UW1G45G_STM32N6570-DK.stldr"
# First Stage Boot Loader
STM32_Programmer_CLI -c port=SWD mode=HOTPLUG -el $DKEL -hardRst -w FSBL/ai_fsbl.hex
# Adjust build path as needed
STM32_Programmer_CLI -c port=SWD mode=HOTPLUG -el $DKEL -hardRst -w build/Application/STM32N6570-DK/Project_sign.bin 0x70100000
# Network parameters
STM32_Programmer_CLI -c port=SWD mode=HOTPLUG -el $DKEL -hardRst -w Model/STM32N6570-DK/network_data.hex
I write a code ( test_bat.bat , please rename test_bat.txt to test_bat.bat ) to program the kit :
but without a succes....
cheers
Emmanuel
2026-03-03 11:59 AM
test_bat.bat
@Echo off
set PROG=C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.300.202508131133\tools\bin\STM32_Programmer_CLI.exe
set EL=C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.300.202508131133\tools\bin\ExternalLoader\MX66UW1G45G_STM32N6570-DK.stldr
set SN=0040003D3234511733353533
rem === FICHIERS GENERES PAR LE SCRIPT PYTHON (VOTRE MODELE) ===
set DEBUG=C:\Users\papam\PycharmProjects\stm32ai-modelzoo-services4\application_code\image_classification\STM32N6\Application\STM32N6570-DK\STM32CubeIDE\Debug
set FSBL=C:\Users\papam\PycharmProjects\stm32ai-modelzoo-services4\application_code\image_classification\STM32N6\FSBL
set MODEL=C:\Users\papam\PycharmProjects\stm32ai-modelzoo-services4\application_code\image_classification\STM32N6\Model\STM32N6570-DK
echo ================================================
echo STM32N6570-DK Flash - VOTRE modele custom
echo ================================================
echo.
echo ATTENTION : Carte doit etre en DEV MODE (BOOT0 gauche)
echo.
echo Fichiers utilises :
echo FSBL : %FSBL%\ai_fsbl.hex
echo Network : %MODEL%\network_atonbuf.xSPI2.bin
echo App : %DEBUG%\STM32N6570-DK_GettingStarted_ImageClassification_signed.bin
echo.
pause
echo === 1/3 Flash FSBL ===
"%PROG%" -c port=swd mode=HOTPLUG sn=%SN% --extload "%EL%" -hardRst -w "%FSBL%\ai_fsbl.hex"
if %errorlevel% neq 0 ( echo ERREUR Flash FSBL ! & pause & exit /b 1)
echo OK
echo.
echo === 2/3 Flash Application (VOTRE application) ===
"%PROG%" -c port=swd mode=HOTPLUG sn=%SN% --extload "%EL%" -hardRst -w "%DEBUG%\STM32N6570-DK_GettingStarted_ImageClassification_signed.bin" 0x70100000
if %errorlevel% neq 0 ( echo ERREUR Flash Application ! & pause & exit /b 1 )
echo OK
echo.
echo === 2/3 Flash Network Data (VOTRE modele) ===
"%PROG%" -c port=swd mode=HOTPLUG sn=%SN% --extload "%EL%" -hardRst -w "%MODEL%\network_data.hex"
if %errorlevel% neq 0 ( echo ERREUR Flash Network Data ! & pause & exit /b 1)
echo OK
echo.
echo ================================================
echo Flash termine avec succes !
echo.
echo ETAPES SUIVANTES :
echo 1. BOOT0 -> gauche (rester en DEV MODE)
echo 2. Eteignez completement le kit
echo 3. Rallumez -> VOTRE application demarre !
echo ================================================
pause
2026-03-04 4:14 AM
Dear all,
the solution is here : https://community.st.com/t5/edge-ai/a-bug-with-stm32cube-ide-2-0-0-and-stm32ai-modelzoo-services/td-p/883573
Cheers
Emmanuel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.