2024-07-26 5:33 AM
Hi,
I'm encountering an issue while porting a trained TensorFlow-Lite model, obtained from a research paper, onto a NUCLEO-F401RE board. The process goes smoothly when analyzing and validating the code on my desktop, generating the code, and downloading it to the board. However, when I attempt to perform a "validate of target," I receive an "Invalid firmware" error (screenshot attached). The model is neural network based on U-Net architecture with shallow structure, single-channel input, and output.
Board used: NUCLEO-F401RE
STM32MX : Version 6.12.0
STM32CubeIDE : Version: 1.16.0
Could you please provide guidance on how to resolve this issue? Any suggestions for modifications or troubleshooting steps would be greatly appreciated.
Thank you!
2024-08-28 1:43 AM
Please verify in the log that the firmware has been correctly compiled and flashed on the target
You can retreive the logs in ~/.stm32cubemx/STM32CubeMX.log
Regards
Daniel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.