cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Tx stucks on 1MHz clock

paduc77
Associate

Hello All,

I'm usin SR6P3 ARM mcu. I have to implement a simple SPI communication with StellarSDK.

When send/receive starts the communication stucks in a while cycle where the code checks Tx queue busyness.

while (queue->tx_busy == SPIQ_QUEUE_TX_BUSY) {
                ;
}
 
Never comes out from this while. The clock is 1MHz.
But if I set the clock lower like 50kHz, then the communication is good.
This is the pin configuration:
/*===========================================================================*/
/*                              SPIQ 0                                       */
/*===========================================================================*/

/* SPIQ0  CLK - PJ12 */
#define SPIQ0_CLK siul2_iopack(SIUL2_PORT_J, SIUL2_PAD_12)
#define SPIQ0_CLK_CFG (SIUL2_MSCR_IO_SSS(0x0B)          | \
                       SIUL2_MSCR_IO_OERC_STRONG        | \
                       SIUL2_MSCR_IO_ODC_PUSH_PULL      | \
                       SIUL2_MSCR_IO_SMC                | \
                       SIUL2_MSCR_IO_ILS_AUTO           | \
                       SIUL2_MSCR_IO_IBE)
/* SPIQ0  SOUT - PK13 */
#define SPIQ0_SOUT siul2_iopack(SIUL2_PORT_K, SIUL2_PAD_13)
#define SPIQ0_SOUT_CFG (SIUL2_MSCR_IO_SSS(0x0E)         | \
                        SIUL2_MSCR_IO_OERC_STRONG       | \
                        SIUL2_MSCR_IO_ODC_PUSH_PULL     | \
                        SIUL2_MSCR_IO_SMC               | \
                        SIUL2_MSCR_IO_ILS_AUTO          | \
                        SIUL2_MSCR_IO_IBE)
/* SPIQ0  SIN - PJ11 */
#define SPIQ0_SIN siul2_iopack(SIUL2_PORT_J, SIUL2_PAD_11)
#define SPIQ0_SIN_CFG (SIUL2_MSCR_IO_SSS(0x00)              | \
                       SIUL2_MSCR_IO_ILS_TTL                | \
                       SIUL2_MSCR_IO_OERC_STRONG            | \
                       SIUL2_MSCR_IO_FILBYPASS              | \
                       SIUL2_MSCR_IO_IBE)

#define SPIQ0_SIN_IOMUX 971u
/* SPIQ0  SIN MSCR.SSS = 0x00 - PJ11 (MSCR Register 971) */
#define SPIQ0_SIN_IOMUX_CFG 1u

/* SPIQ0  CS0 - PJ8 */
#define SPIQ0_CS0 siul2_iopack(SIUL2_PORT_J, SIUL2_PAD_8)
#define SPIQ0_CS0_CFG (SIUL2_MSCR_IO_SSS(0x08)         | \
                       SIUL2_MSCR_IO_OERC_STRONG       | \
                       SIUL2_MSCR_IO_ODC_PUSH_PULL     | \
                       SIUL2_MSCR_IO_SMC               | \
                       SIUL2_MSCR_IO_ILS_AUTO          | \
                       SIUL2_MSCR_IO_IBE)
#define SPIQ0_CS0_IOMUX 969u
#define SPIQ0_CS0_IOMUX_CFG 2u
 
And this is the SPI config:
    spiq_pcs_default_level(&spiqd_0, SPIQ_PCS_0, SPIQ_SIGNAL_LEVEL_HIGH);
    spiq_start(&spiqd_0);

    queue_SBC_PFS273 = spiq_queue_allocate(&spiqd_0);
    tac_SBC_PFS273 = spiq_tac_allocate(&spiqd_0);

    spiq_queue_mode(queue_SBC_PFS273, SPIQ_QUEUE_MODE_PRIO_5);
    spiq_queue_mode(queue_SBC_PFS273, SPIQ_QUEUE_MODE_TX_SYNCHRONOUS);
    spiq_queue_mode(queue_SBC_PFS273, SPIQ_QUEUE_MODE_TX_CPU);
    spiq_queue_mode(queue_SBC_PFS273, SPIQ_QUEUE_MODE_RX_SYNCHRONOUS);
    spiq_queue_mode(queue_SBC_PFS273, SPIQ_QUEUE_MODE_RX_CPU);

    /*Trasfer control registers setup*/
    uint32_t leading_delay = spiq_tac_mode_set_delay(tac_SBC_PFS273, SPIQ_TAC_LEADING_DELAY, 800UL);
    uint32_t trailing_delay = spiq_tac_mode_set_delay(tac_SBC_PFS273, SPIQ_TAC_TRAILING_DELAY, 800UL);
    uint32_t inter_word_delay = spiq_tac_mode_set_delay(tac_SBC_PFS273, SPIQ_TAC_INTER_WORD_DELAY, 200UL);
    uint32_t next_frame_delay = spiq_tac_mode_set_delay(tac_SBC_PFS273, SPIQ_TAC_NEXT_FRAME_DELAY, 200UL);
    effective_baud_rate = spiq_tac_mode_set_baud_rate(tac_SBC_PFS273, 50000UL, SPIQ_TAC_BAUD_DOUBLE_OFF);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_CLOCK_INACTIVE_LOW); //(CPOL = 0)
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_CLOCK_PHASE_HIGH); // (CHPA = 1)
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_SHIFT_MSB_FIRST);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_FRAME_SIZE_32_BITS);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_SW_TRIGGER_ENABLE);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_DATA_IN_RXFIFO);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_CRC_DISABLE);
    spiq_tac_set_pcs(tac_SBC_PFS273, SPIQ_PCS_0);
    spiq_tac_mode(tac_SBC_PFS273, SPIQ_TAC_CONT_PCS_DISABLED);
 
Does anybody know what should be the problem. Thanks.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

Which version of StellarSSDK do you use ?

(the last one in 5.0.0)

SR6P7 is not Mass Market , i recommend to contact your FAE

         Best regards

                    Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Hello ,

Which version of StellarSSDK do you use ?

(the last one in 5.0.0)

SR6P7 is not Mass Market , i recommend to contact your FAE

         Best regards

                    Erwan

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.