2015-06-18 3:49 AM
Hello,
I am using SPC5Stuido and the output file is generated as out.elf or out.hex etc. It is the default setting. I want to change it as per project need. From which project settings can I change the output file name? Where is it documented?Thanks in advance.Mike.2015-06-18 5:35 AM
Hi,
In the platform component, under ''Build'', there is ''Application Name''. The default is ''out''. Giovanni2015-06-18 7:43 AM
Thanks Giovanni. I missed that section, was looking under project properties.
Mike.2015-06-18 8:03 AM
In general in SPC5Studio it is better to assume that it is in the configuration. Project properties do not do much because projects are Makefile-based and the makefile is generated.
GiovanniWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.