2021-05-07 2:45 AM
Hi All ,
I flashed the board Spc584b-Disp with a SW that had a watchdog reset happening .
When I repower the Board and try to connect to it to reflash ,the RESET LED4 is alawys ON ,and the UDE gives an error PpcJtagTargIntf: No JTAG client found !
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
No JTAG client found !
Please check:
- target power supply
- JTAG cable connection
- target configuration
I know it is not the UDE STK 5.2 Problem because I reinstalled the drivers and the UDE STK and I can connect to other Spc58 Boards using it .
The problem is with the Board ,I can see the SW running at power ON (LEDS Indication) and then going through WDG RESET forever .
Is there a way I can fix this ?
All Board Jumpers are in Default setting.
Solved! Go to Solution.
2021-05-11 1:39 AM
Hello R.M. ,
maybe you are in Reset Escalation , Could you hold reset button and try to connect in order to take the hand on PLS ?
Best Regards
Erwan
2021-05-11 1:39 AM
Hello R.M. ,
maybe you are in Reset Escalation , Could you hold reset button and try to connect in order to take the hand on PLS ?
Best Regards
Erwan
2021-05-11 3:22 AM
Thank you ,That actually Worked !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.