cancel
Showing results for 
Search instead for 
Did you mean: 

SPC564A compatibility SPC563M

armitage.richard
Associate II

SPC564A datasheet promises compatability.

Does that mean I can swap out SPC563M with SPC564A.

Set target addresses in firmware, build and install, and all runs hunky dory?

2 REPLIES 2
Erwan YVIN
ST Employee

Hello Richard ,

I recommend to check in SPC5Studio Tools Suite

to converge from SPC563M to SPC64A 

(Set target addresses in firmware, build and install)

I have to take care tour pinmap configuration and the IP Iused 

  Best Regards

                 Erwan

 

Thank you Erwan.

I am unfamiliar with SPC5Studio Tools Suite, I will have ago.

Datasheet promises "3. Pinout compatible with STMicroelectronics’ SPC563M64 devices." for the LQFP176(3).

"I have to take care tour pinmap configuration and the IP Iused " I must ensure any of the new features will not disturb the pin out assignment for the backwards compatibility.

As an aside odd that; spc564a70l7.pdf, September 2013 Doc ID 18078 Rev 4, is still "This is preliminary information on a new product now in development or undergoing evaluation. Details are subject to change without notice."

And imperial air flow 200ft/min ~ 1m/s I guess if you are a 2nd source that happens. Or more likely strict following of JEDEC JESD51-3 from the late 90s. Lets not miss Mars!

Unless there is more guidance lets close.

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.