2019-04-01 1:04 AM
Hi there,
I've downloaded the SPC5-CRYP-LIB from the ST website. It says that it should be supported for the whole SPC5xx family, with hardware support only enabled for the SPC560B/C MCU. I am trying to import this plugin for the SPC560B54, but SPCStudio is saying it is incompatible with my project. When I try to import it anyway, it fails to compile. Is there anything I'm doing wrong here?
Solved! Go to Solution.
2019-04-01 6:38 AM
Hello ,
The ST Website is outdated for SPC5-CRYP-LIB
Better to use the update site mecanism in SPC5Studio
http://download.spc5studio.com/updates
Please Add for the dependencies
http://community.spc5studio.com
More information on
http://download.spc5studio.com/
Best regards
Erwan
2019-04-01 6:38 AM
Hello ,
The ST Website is outdated for SPC5-CRYP-LIB
Better to use the update site mecanism in SPC5Studio
http://download.spc5studio.com/updates
Please Add for the dependencies
http://community.spc5studio.com
More information on
http://download.spc5studio.com/
Best regards
Erwan
2019-04-01 7:11 AM
Hello,
Thank you for the quick reply! I have a few additional questions. Has the SPC5-Studio download link been taken down on the website? I have a colleague who wants to download it but the link seems to redirect to the same page.
Also, when I create a new project and want to debug it with UDE STK, only the breakpoints view comes up (so no source files, functions, ...). When I copy my code over to an example project (f.e. the CAN example), then the UDE software shows all functions, source files and gives me an option to flash the firmware. Why is that?
2019-04-04 7:14 AM
Hello ,
For the first point , yes , the download link was broken.
i think that it is ok from now.
UDE STK is using in order to flash and debug your device.
on a classical debug.wsx (debug workspace)
PLS UDE is going to display the Memtool Windows (Flash)
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.