2015-02-09 11:33 PM
when I use DSPI , I send two frames 16bits per frame, and I monitor that there is a pulse inter frame on MOSI pin (suppose I send two frames 0x00000000 ), it is very strange , I checked step and step,when I set MOSI pin as SIU.PCR[38].R=0x0604 or 0x06xx; MOSI will change to high value;
So I guess the interframe high level shown is due to MOSI return to default value high. But can I set default value of MOSI as low level value ? --Note , there is no external pull up on MOSI , and when I configure MOSI as output low , the pin still show highlevel.2015-02-10 9:58 AM
Hi,
It is possible it is just an issue with the tDT delay time, see the Reference Manual. You need to program the PDT, PASC, PCSSCK fields of the CTAR register(s) in order to program the inter-frame time. Note that all the fields in the CTAR register are quite important and must be programmed correctly or you will get strange results. Giovanni2015-02-10 5:37 PM
2015-02-11 4:36 AM
HI,
MOSI cannot be directly controlled, its idle state is always high. You could switch it to GPIO and control it ''manually'' but are you sure it is really required? Giovanni2015-02-11 5:33 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.