2023-11-28 6:12 AM - edited 2023-11-28 6:50 AM
I configured the SWT to Generate an interrupt on an initial time-out, reset on a second consecutive time-out.
The interrupt is well raised on the initial time-out.
The problem is that the reset is not occurred in the next time-out.
here the initialisation sequence of SWT :
/* Disable Software Lock */
SWT_2->SR.B.WSC = 0xC520U;
SWT_2->SR.B.WSC = 0xD928U;
/* Wait until Software Lock is disabled */
while (1U == SWT_2->CR.B.SLK) {/* Empty while */}
/* disable the SWT */
SWT_2->CR.B.WEN = 0U;
SWT_2->CR.B.FRZ = 0U;
SWT_2->CR.B.SMD = 0U;
SWT_2->CR.B.WND = 0U;
SWT_2->CR.B.STP = 1U;
SWT_2->CR.B.RIA = 0U;
SWT_2->IR.B.TIF = 1U;
SWT_2->TO.B.WTO = 0x00088B80U;
/* Enable the SWT */
SWT_2->CR.B.WEN = 1U;
I tried also Generate a reset on a time-out(without interrupt) but also the CPU does not reset
PS: To have the time out I'm in empty while(1) {};
I missed something in configuration ? Thank you for your help
Solved! Go to Solution.
2023-12-05 1:02 AM
Issue resolved by configuring FCCU to request a functional reset when the SWT2 triggers the fault 18 to the
FCCU by code below :
/* enter the CONFIG mode */
FCCU.TRANS_LOCK.R = 0x000000BCU; /* write the TRANSKEY */
/* configure the CONFIG timeout */
FCCU.CFG_TO.R = 0x00000006U;
FCCU.CTRLK.R = 0x913756AFU; /* key for OPERATION 1 */
/* set the FCCU into the CONFIG state OP1 */
FCCU.CTRL.R = 0x00000001U;
/* wait for operation finalization */
while (FCCU.CTRL.B.OPS != FCCU_OPS_SUCCESS);
/* enable HW recoverable fault to generate Reset on SWT_2 fault */
FCCU.RF_CFG[0].B.RFC18 = 0x0U;
/* long Functional Reset as reaction to the SWT_2 refresh fault */
FCCU.RFS_CFG[1].B.RFSC2 = 0x2U;
/* move to FAULT state when SWT_2 expires to generate Reset */
FCCU.RF_E[0].B.RFE18 = 0x1U;
/* enter back to the NORMAL mode */
FCCU.CTRLK.R = 0x825A132BU; /* key for OPERATION 2 */
/* set the FCCU into the NORMAL state OP2 */
FCCU.CTRL.R = 0x00000002U;
/* wait for operation finalization */
while (FCCU.CTRL.B.OPS != FCCU_OPS_SUCCESS);
2023-12-05 1:02 AM
Issue resolved by configuring FCCU to request a functional reset when the SWT2 triggers the fault 18 to the
FCCU by code below :
/* enter the CONFIG mode */
FCCU.TRANS_LOCK.R = 0x000000BCU; /* write the TRANSKEY */
/* configure the CONFIG timeout */
FCCU.CFG_TO.R = 0x00000006U;
FCCU.CTRLK.R = 0x913756AFU; /* key for OPERATION 1 */
/* set the FCCU into the CONFIG state OP1 */
FCCU.CTRL.R = 0x00000001U;
/* wait for operation finalization */
while (FCCU.CTRL.B.OPS != FCCU_OPS_SUCCESS);
/* enable HW recoverable fault to generate Reset on SWT_2 fault */
FCCU.RF_CFG[0].B.RFC18 = 0x0U;
/* long Functional Reset as reaction to the SWT_2 refresh fault */
FCCU.RFS_CFG[1].B.RFSC2 = 0x2U;
/* move to FAULT state when SWT_2 expires to generate Reset */
FCCU.RF_E[0].B.RFE18 = 0x1U;
/* enter back to the NORMAL mode */
FCCU.CTRLK.R = 0x825A132BU; /* key for OPERATION 2 */
/* set the FCCU into the NORMAL state OP2 */
FCCU.CTRL.R = 0x00000002U;
/* wait for operation finalization */
while (FCCU.CTRL.B.OPS != FCCU_OPS_SUCCESS);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.