2016-12-07 12:13 AM
Hello,
I would like to make a native Linux build of the ppc-freevle-eabi toolchain that is shipped with SPC5Studio; the toolchain comes with a readme.txt with some release notes, but it does not state the origin or where sources can be found.
Can anyone shed some light on this? Are the sources available as a whole, and if not, are the changes made to the default 4.9.2 gcc available somewhere?
Thank you,
2016-12-07 12:57 AM
Hello Gert ,
The gcc
ppc-freevle-eabi toolchain
(4.9.2) is coming from NXP-Freescale side.the source code is coming from nxp community.
https://community.nxp.com/docs/DOC-333045
We are using the similar core on PowerPC microcontrollers (MPC56-SPC56)
Linux version is working well.
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.