2016-10-27 5:46 AM
Hi,
I need to work on old project created using SPC5Studio V3.5. Project is created using Wizards. When I open same project using V5.0, the 'Configuration.xml' is showing some error (red cross against file name). If I try to generate new code using 'Configuration.xml' it is giving following error messages
hal_lld.h 1.0.0.201609071703 : ...CAN NOT APPLY THE PATCH...
FlashMap.h 1.0.0.201609061636 : ...CAN NOT APPLY THE PATCH...
Am I doing something wrong?
First time I am using SPC5Studio
2016-11-07 1:34 AM
Hi,
there should be a problem importing old project into new 5.0. some files massively changed , so it could be a prolem patching new files with old patch. My suggestion is to create a brand new project in 5.0 and then reapply the patches on those files. RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.