2019-05-19 11:02 PM
Dear
I am using SPC5Studio version 5.8.1 and SPC570S.
I want to fill the output(.mot) file with 0xFF memory.
In additional, I want to make hex file a contiguous address.
Below is my output.mot file with non-contiguous addresses.
S214FD07D0010E01220136014A015E000A00000333C4
S214FD07E00100000100000199010000000000001C4E
S20EFD07F00000007800001000000174
S206FD07FA0000FB
I need help.
Thank you in advance.
Solved! Go to Solution.
2019-08-13 8:03 AM
Hello ,
With PLS , i do not think that it is possible
You should use by Software Implementation
Best regards
Erwan
2019-08-13 8:03 AM
Hello ,
With PLS , i do not think that it is possible
You should use by Software Implementation
Best regards
Erwan
2019-08-13 8:16 AM
The .MOT file format isn't unduly complicated, should be something a C coder could do pretty quickly. You could read the content into a preallocated and filled buffer, and then re-export as a continuous/linear image. Tools like SRECORDS too
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.