2021-10-16 7:40 PM
Solved! Go to Solution.
2021-12-02 6:03 AM
Hello Apant ,
1) Yes ,
10 and 100, Mbps data transfer rates with the following PHY interfaces:
– IEEE 802.3-compliant MII interface to communicate with an external Fast Ethernet PHY
– RMII interface to communicate with an external Fast Ethernet PHY (ok for RTL8201F)
2) In discovery board we are using CI Ethernet
DP83848YB/NOPB
We have no library on this IC.
you have to create it.
anyway , you can refer to the application :
SPC58ECxx_RLA Network Ping Test Application for Discovery
(Network component as example)
Best Regards
Erwan
2021-12-02 6:03 AM
Hello Apant ,
1) Yes ,
10 and 100, Mbps data transfer rates with the following PHY interfaces:
– IEEE 802.3-compliant MII interface to communicate with an external Fast Ethernet PHY
– RMII interface to communicate with an external Fast Ethernet PHY (ok for RTL8201F)
2) In discovery board we are using CI Ethernet
DP83848YB/NOPB
We have no library on this IC.
you have to create it.
anyway , you can refer to the application :
SPC58ECxx_RLA Network Ping Test Application for Discovery
(Network component as example)
Best Regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.