cancel
Showing results for 
Search instead for 
Did you mean: 

FlashErase/FlashProgram not working with any optimization level (-Os size/-O1 general/-O2 speed/-O3 fast) except -O0 none.

DMA
Associate II

Hi, I am working on SPC58NG84E7 bootloader. I have Bootloader code(at 0x00FC0000) with which i am using "FlashErase" API to Erase Flash Memory block at 0x00FF0000 with "-Os size" Optimization But its not working. Also, I tried putting breakpoint to the next line after erase, but breakpoint does not hit. Looks like its stuck in the execution.

I tried all other optimizations as well but same result.

Also, without optimization (NONE(-O0)) its working fine. 

Same result is for "FlashProgram" API.

What could be the issue here?

Please help me resolve the issue.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ODOUV.1
ST Employee

Hello,

your parameters are good.

Would you please check it could be the same issue than this one :

Flash Erase for SPC58NG84E7 is not working (st.com)

Best Regards,

-Olivier

View solution in original post

14 REPLIES 14
ODOUV.1
ST Employee
DMA
Associate II

Hi Oliver,

Thanks for your reply. But that issue is different than what i am facing. It didn't work.

I am getting unhandled exception.

Any other suggestions??

Thanks and Regards

Deepesh

ODOUV.1
ST Employee

Hello Deepesh,

I have no over idea with your optimization level issue.

I will forward your concern to the Flash Driver expert and let you know any feedback.

Best Regards,

-Olivier

ODOUV.1
ST Employee

Hello,

how are you selecting your low block to erase at 0xFF_0000 ?

do you use lowBlockSelect 0x200 ? and other select to 0 ?

BRs,

-Olivier

DMA
Associate II

Configuration for flash is as follows:

SSD_CONFIG FLSHM_ssdConfig = {

C55_REG_BASE, /* C55 control register base */

MAIN_ARRAY_BASE, /* base of main array */

{ 0, 0, 0 }, /* blocks info of low address space */

{ 0, 0, 0 }, /* blocks info of mid address space */

{ 0, 0, 0 }, /* blocks info of high address space */

0, /* number of blocks in 256K address space */

UTEST_ARRAY_BASE, /* base of UTEST array */

TRUE, /* interface flag indicate main or alternate interface */

0x80,/* programmable size */

FALSE /* debug mode selection */

};

Below steps to get flash block erased-

#define LOWBLOCKSELECT 0x00000200U (0x00FF0000)

#define MIDBLOCKSELECT 0x00000000U

#define HIGHBLOCKSELECT 0x00000000U

 /* Unlock the requested block for Erase operation */

nLargeBlockSelect.firstLargeBlockSelect = 0;

nLargeBlockSelect.secondLargeBlockSelect = 0;

SetLock(&FLSHM_ssdConfig, C55_BLOCK_LOW, UNLOCK_ALL_BLOCKS);

/* Erase the requested block */

Return_Val = FlashErase(&FLSHM_ssdConfig, C55_ERASE_MAIN, LOWBLOCKSELECT,

MIDBLOCKSELECT, HIGHBLOCKSELECT, nLargeBlockSelect);

if(Return_Val == C55_OK)

{

 while(C55_INPROGRESS == FlashCheckStatus(&FLSHM_ssdConfig, C55_MODE_OP_ERASE, &opResult, &FLSHM_eraseCtxData));

 /* Erase is successful */

}

else

{

/* Erase failed */

}

ODOUV.1
ST Employee

Hello,

your parameters are good.

Would you please check it could be the same issue than this one :

Flash Erase for SPC58NG84E7 is not working (st.com)

Best Regards,

-Olivier

ODOUV.1
ST Employee

Could you try this Load in RAM configuration ? (in SPC58xGxx RLA Platfrom->runtime settings)0693W00000JNilIQAT.png 

BRs,

-Olivier

Hi Oliver

Yes Its similar to the issue that I am facing currently.

Current solution is to put your program in RAM.

I asked for an analysis from R&D.

I will keep you informed.

Best Regards,

-Olivier

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.