2014-09-13 11:39 AM
Hi,
I have tried to
compile
an example
with the
SPC5Studio
Wizard
and
get the following
error
s: 20:36:34 **** Incremental Build of configuration Default for project ChibiOS-RT SPC56ELxx Test Application for DiscoveryPlus **** make -j4 all 0 [main] sh 1656 sync_with_child: child 3980(0x188) died before initialization with status code 0xC0000142 14 [main] sh 1656 sync_with_child: *** child state waiting for longjmp /bin/sh: fork: Resource temporarily unavailable Compiling boot.s Compiling crt0.s Compiling ivor.s Compiling vectors.s C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201409031447/component/lib/src/boot.s:26:0: fatal error: opening dependency file .dep/boot.o.d: No such file or directory compilation terminated. make: *** [build/obj/boot.o] Error 1 make: *** Waiting for unfinished jobs.... C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201409031447/component/lib/src/crt0.s:1:0: fatal error: opening dependency file .dep/crt0.o.d: No such file or directory C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.kernel.port.gcc.spc56elxx_2.6.4.201409031447/component/lib/src/ivor.s:42:0: fatal error: opening dependency file .dep/ivor.o.d: No such file or directory compilation terminated. C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.kernel.port.gcc.spc56elxx_2.6.4.201409031447/component/lib/src/vectors.s:1:0: fatal error: opening dependency file .dep/vectors.o.d: No such file or directory compilation terminated. compilation terminated. make: *** [build/obj/ivor.o] Error 1 make: *** [build/obj/crt0.o] Error 1 make: *** [build/obj/vectors.o] Error 1 20:36:35 Build Finished (took 810ms) The files are avaliabe in the directories. OS: Windows 8.1, 64bit very frustrating ;(2014-09-14 1:24 PM
Update:
if i set the enviroment variables to ''replace native enviroment with specific one'' i get the follingwing error: bash.exe: warning: could not find /tmp, please create! Compiling boot.s C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201409031447/component/lib/src/boot.s:1:0: internal compiler error: initialising license system No license for product (-1) (Product: ppc-free-gcc, Version: 2013.01) I also add the RLM_LICENSE (C:\SPC5Studio\licenses\) variable to the Enviroment settings2014-09-15 2:35 AM
Hello Virus2k,
Normally , you should have ''Append Variables to native environment'' not replace ''replace native enviroment with specific one''.your environment variables should have :==> RLM_LICENSE should contain c:\SPC5Studio\licencesDo you update your environment variables ?do you copy the file ''licence.lic'' in c:\SPC5Studio\licences ?licence.lic is linked to your MAC address==> the PATH is selected by CDT Environment in SPC5STudio by defaultYour first issue is a make error ..make -j4 all 0 [main] sh 1656 sync_with_child: child 3980(0x188) died before initialization with status code 0xC0000142 14 [main] sh 1656 sync_with_child: *** child state waiting for longjmp/bin/sh: fork: Resource temporarily unavailableif you click , on ''replace native enviroment with specific one'' (not recommended because with bad settings we can use an other make (cygwin for example) not compliant with our env)You should use the make inside SPC5Studio not the cygwin make.c:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.gnu_1.0.0.201306281422\gnutools\for the compiler :c:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\bin\Anyway , We are checking if there is a side effect on Windows 8.1. Best Regards ErwanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.