2014-08-04 8:22 AM
Are there any example projects for the SPC564A on the SPC56xxMB EVAL board that show how to use external RAM?
If not complete projects, any code snippets or even hints or advice?ThanksKevinSolved! Go to Solution.
2014-08-08 8:13 AM
Hello Kevin ,
On the application wizard , there are 5 test applications :SPC564Axx OS-Less CAN Test ApplicationSPC564Axx OS-Less DSPI Example ApplicationSPC564Axx OS-Less eQADC Example ApplicationSPC564Axx OS-Less ICU-PWM Test ApplicationSPC564Axx OS-Less Test ApplicationI am checking with experts about your requests. Best regards2014-08-08 8:13 AM
Hello Kevin ,
On the application wizard , there are 5 test applications :SPC564Axx OS-Less CAN Test ApplicationSPC564Axx OS-Less DSPI Example ApplicationSPC564Axx OS-Less eQADC Example ApplicationSPC564Axx OS-Less ICU-PWM Test ApplicationSPC564Axx OS-Less Test ApplicationI am checking with experts about your requests. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.