2018-06-07 10:14 PM
I am working on SPC563M64 controller. I have started working on shadow flash now. But during testing of shadow flash code I got debug port fail error while trying to connect to controller. I think the board is permanently reset and I am not able to connect to my board again. What can I do ? I have also tried the sequence of commands in a sequence listed below but still I was not able to connect to controller :
1. system.option.cpu
2.SYStem.Option.KEYCODE 0xFEEDFACECAFEBEEF
3. system.up.
Please tell me what is this issue is ?
#spc5x2018-06-08 12:59 AM
Hello Ankit ,
You are using TRACE32 lautechbach ..
Have you updated the shadow flash ?
could you try to click on Reset Button of your board in trying to connect the debugger in the same time .
Maybe , there is a sort of reset escalation.
Best Regards
Erwan
2018-06-08 3:31 AM
Yes I updated shadow flash and after that I did reset and from then this problem is coming.
I tried to connect to board while press the reset button at the same time but error showed that ' target reset failed '.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.