cancel
Showing results for 
Search instead for 
Did you mean: 

Can you help out a random student in need of help with his bachelors degree CAN bus task?

MPree.1
Associate

I am doing my bachelors degree and have a task to get two boards communicating using the CAN bus. I just got the boards and they pretty much said "have at it" without any prior knowledge.

By now i know most of the really basic stuff about the CAN bus and SPC5Studio but I don't know where to start and what to read. The boards that I got are aek-mot-3p99081 (with the motor) and spc58ec-disp. I also downloaded all of the necessary stuff for the SPC5Studio such as AutoDevKit, MCTK etc. I underastand that i need two terminating resistors and then connect the boards?

I am supposed to load the programs to the board and test them out seperately and then start testing the communication between them using the CAN bus. How can i do it and where to start? And might there be a really bored expert that can help a student out for some weird reason with a call or explanation.

Thank you for reading :).

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Mpree ,

Welcom to the SPC5Studio,

all the autodevkit sw stuffs are in the following update site,

http://autodevkit.spc5studio.com/

installable in SPC5Studio 6.0

Best Regards

Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Hello Mpree ,

Welcom to the SPC5Studio,

all the autodevkit sw stuffs are in the following update site,

http://autodevkit.spc5studio.com/

installable in SPC5Studio 6.0

Best Regards

Erwan

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.